Hello:
We'd like to use the DM6433's PCI (and/or USB) for communcation with other processors.
Are these communications standards supported via DSP/BIOS or do we need to use linux on the processor?
Thanks,
--B
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
You should have DSP/BIOS for both of these based on our DM643x EVM; however, it worth noting that DM6433 device does not support USB; this was supported on our EVM via external USB Phy.
The steps for using the PCI sample application on the DM6437 are given on page 22 of the PSP_User_Guide.pdf file found within C:\dvsdk_1_11_00_00\pspdrivers_1_10_00\docs\dm6437. Note that the host side of the driver is for a Linux machine.