This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: Bitbake build error

Part Number: PROCESSOR-SDK-AM335X

Tool/software: Linux

Hi,

I need your support regarding bitbake of AM335x Processor SDK.

I am trying to build the SDK based on "Using the snapshot of the source packages in Processor SDK release" of Processors SDK Building The SDK ( http://processors.wiki.ti.com/index.php/Processor_SDK_Building_The_SDK ) .

But, When I execute the command "MACHINE=am335x-evm bitbake arago-core-tisdk-image",  host is freezed. Please see the below.

==============================================================================================================

yamamoto@ubuntu:~/tisdk/build$ MACHINE=am335x-evm bitbake arago-core-tisdk-image
Loading cache: 100% |############################################################################| Time: 0:00:05
Loaded 3799 entries from dependency cache.
Parsing recipes: 100% |##########################################################################| Time: 0:00:03
Parsing of 3033 .bb files complete (3030 cached, 3 parsed). 3800 targets, 571 skipped, 0 masked, 0 errors.
WARNING: No recipes available for:
  /home/yamamoto/tisdk/sources/meta-openamp/recipes-bsp/device-tree/device-tree-generation_%.bbappend
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION        = "1.32.0"
BUILD_SYS         = "x86_64-linux"
NATIVELSBSTRING   = "Ubuntu-14.04"
TARGET_SYS        = "arm-linux-gnueabi"
MACHINE           = "am335x-evm"
DISTRO            = "arago"
DISTRO_VERSION    = "2017.10"
TUNE_FEATURES     = "arm armv7a vfp thumb neon       callconvention-hard"
TARGET_FPU        = "hard"
meta-processor-sdk = "HEAD:eaac60268857bc56bf89625df93935a272b63341"
meta-ros          = "HEAD:e01c6ace0d4f9d700449edad3781e9cd505b5e10"
meta-arago-distro
meta-arago-extras = "HEAD:d34c861f846f35d089e1caf224ec43079be7b202"
meta-browser      = "HEAD:26d50665e2f7223c5f4ad7481a8d2431e7cb55fb"
meta-openamp      = "HEAD:8a214032bfb7e8124bc1485c70c69f7d60abb819"
meta-qt5          = "HEAD:2c9f0e4eb0e9097f6f872ec1e1d81768a8ab5f1b"
meta-networking  
meta-ruby        
meta-python      
meta-oe          
meta-gnome       
meta-multimedia   = "HEAD:b40116cf457b88a2db14b86fda9627fb34d56ae6"
meta-ti           = "HEAD:351ccf1928a18c2b69fd19b09b980c9aa3af2e26"
meta-linaro-toolchain
meta-optee        = "HEAD:5d2cb685217794293ea2bab18d7e62019c329d06"
meta              = "HEAD:1718f0a6c1de9c23660a9bebfd4420e3c4ed37e6"

Initialising tasks: 100% |#######################################################################| Time: 0:00:51
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
Currently  1 running tasks (2771 of 9058)  30% |###################                                            |
0: qtwebengine-5.7.1+gitAUTOINC+9cc97f0c63_b3c79e92f0-r0.arago0 do_compile - 1780s (pid 92655)

===================================================================================================

I tried to execute this command few times. But always it is stopped at 2771 of 9058 tasks.

I don't know why this task is stopped. 

My environment is the below:

Ubuntu 140.04.5

Processor SDK version : 04.0.00.09

Now I have 150GB disk space for ubuntu in vmware. And approximately 120GB already is spent.

also the swap size is 20GB.

Please advise me.

Best regards,

Michi

  • Hello,

    1.I would recommend you to increase the size >200GB.
    2. Some of the tasks needs more time to compile. If you are wondering why only this task is running probably the another one depends on this one.
    3. You could try to run only MACHINE=xxx bitbake qtwebengine

    BR
    Margarita