Part Number: AM5728
Tool/software: TI-RTOS
Hi there,
Using AM5728/C66x/TI-RTOS, the AM5728 communicates with a FPGA by PCIe and It works well. However, I test ECRC test function but It doesn't work.
(AM5728 supposed to send a corrupted TX TLP, FPGA couldn't checked it).
To corrupt a PCIe TX TLP, I used PCIECTRL_TI_CONF_DIAG_CTRL register.
My questions are:
1. ECRC is always enabled?
2. My test code is shown below. Is this code send a corrupted TX TLP?
...
while(1)
{
Task_sleep(1000);
irqRaised1 = 0;
retVal = pcieRcSendECRC(handle);
drvInst->shadowRegs->ESR = 1UL << 1; //send PCIe TX TLP by DMA
while (!irqRaised1);
}
...
}
pcieRet_e pcieRcSendECRC (Pcie_Handle handle)
{
pcieRegisters_t regs;
pcieTiConfDiagCtrlReg_t eCRCAssert;
pcieRet_e retVal;
PCIE_logPrintf ("RC sending ECRC to EP\n");
/* Now send ECRC error TLP */
memset (®s, 0, sizeof(regs));
memset (&eCRCAssert, 0, sizeof(eCRCAssert));
/* Read the current value */
regs.tiConfDiagCtrl = &eCRCAssert;
retVal = Pcie_readRegs (handle, pcie_LOCATION_LOCAL, ®s);
if (retVal != pcie_RET_OK){
PCIE_logPrintf("Can't read ECRC control regs in ticonf\n");
return pcie_RET_UNSUPPORTED;
}
if (eCRCAssert.invEcrc){
PCIE_logPrintf("ECRC control already asserted\n");
}
else{
/* Send it */
eCRCAssert.invEcrc = 1U;
retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, ®s);
if (retVal != pcie_RET_OK){
PCIE_logPrintf("Can't write Ecrc control regs in ticonf\n");
return pcie_RET_UNSUPPORTED;
}
else{
PCIE_logPrintf("ECRC asserted\n");
}
}
return pcie_RET_OK;
}
|
Thank you in advance
Sangwook Han