This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AM5716: McASP digital loopback

Part Number: AM5716

Tool/software: TI-RTOS

Hi,

I am using  EDMA to transfer data between McASP and and my ping pong buffer using EDMA on AM5716. I have verified the the data from my output buffer to McASP is working( I see the data on scope). since there is no data availabe on McASP input pin at this moment, so I'd like use McASP digital loopback to check if EDMA working in receiving direction.  I have set DLBEN =1 in DLBCTL register. but I did not see the data send from EDMA back to my input buffer. I chceked the EDMA receiving is working( I see the TCC 0, and 1  for channel 0 for receiving). I wonder what else I can check if the data is loopped back from McASP?

Thanks in advance!

Ron