Part Number: TMDSICE3359
Other Parts Discussed in Thread: SYSBIOS, AM3359
Tool/software: TI-RTOS
Hello everyone,
I am a beginner with TI CCS and started to dive into RTOS-World with the TMDSICE3359 V2 device.
My problem is to build a simple project which uses GPIO driver with usage of the TI toolset (ARM Compiler, ARM Linker). However, the same SysBios.cfg works with a project which uses gnu toolset (GNU Compiler, GNU Linker).
I will describe my environemnt, the steps I have done, the SysBios configuration and the build output of both projects. Additionally I have some questions.
I worked through
processors.wiki.ti.com/.../Processor_SDK_RTOS_Software_Developer_Guide
1. Environment
I set up my environment with CCS 7.4, pdk_am335x_1_0_10, xdctools_3_50_04_43_core. I rebuilt the PDK sucessfully.
All the PDK example projects, which are loacted under /home/thomas/ti/pdk_am335x_1_0_10/packages/MyExampleProjects build an run fine!
All the CCS-Project templates works fine (with TI-Compiler or GNU-Compiler used).
That said, I wanted to understand how SysBios works and how it needs to get configurated in a correct way. I can't find much details about this on the TI website and wikis.
2. Steps
My plan was to start with a SYS/BIOS-Typical project template, and add minimal configurations to be able to interface the GPIOs on the board.
2.1 Created Project Template (New CCS Project, Compiler Version: TI v16.9.6.LTS, Target: ICE_AM3359). Building at this stage was successfull.
I investigated some threads here in the forum, and found out that I probably need the "OSAL-Layer", the "CSL-Layer" and maybe the UART and I2C package to use and initialize the GPIO drivers.
2.2 Change to app.cfg
So my complete app.cfg looks like this:
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Error = xdc.useModule('xdc.runtime.Error');
var Log = xdc.useModule('xdc.runtime.Log');
var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
var Main = xdc.useModule('xdc.runtime.Main');
var Memory = xdc.useModule('xdc.runtime.Memory')
var SysMin = xdc.useModule('xdc.runtime.SysMin');
var System = xdc.useModule('xdc.runtime.System');
var Text = xdc.useModule('xdc.runtime.Text');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
var Swi = xdc.useModule('ti.sysbios.knl.Swi');
var Task = xdc.useModule('ti.sysbios.knl.Task');
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
var Hwi = xdc.useModule('ti.sysbios.hal.Hwi');
/*
* Uncomment this line to globally disable Asserts.
* All modules inherit the default from the 'Defaults' module. You
* can override these defaults on a per-module basis using Module.common$.
* Disabling Asserts will save code space and improve runtime performance.
Defaults.common$.diags_ASSERT = Diags.ALWAYS_OFF;
*/
/*
* Uncomment this line to keep module names from being loaded on the target.
* The module name strings are placed in the .const section. Setting this
* parameter to false will save space in the .const section. Error and
* Assert messages will contain an "unknown module" prefix instead
* of the actual module name.
Defaults.common$.namedModule = false;
*/
/*
* Minimize exit handler array in System. The System module includes
* an array of functions that are registered with System_atexit() to be
* called by System_exit().
*/
System.maxAtexitHandlers = 4;
/*
* Uncomment this line to disable the Error print function.
* We lose error information when this is disabled since the errors are
* not printed. Disabling the raiseHook will save some code space if
* your app is not using System_printf() since the Error_print() function
* calls System_printf().
Error.raiseHook = null;
*/
/*
* Uncomment this line to keep Error, Assert, and Log strings from being
* loaded on the target. These strings are placed in the .const section.
* Setting this parameter to false will save space in the .const section.
* Error, Assert and Log message will print raw ids and args instead of
* a formatted message.
Text.isLoaded = false;
*/
/*
* Uncomment this line to disable the output of characters by SysMin
* when the program exits. SysMin writes characters to a circular buffer.
* This buffer can be viewed using the SysMin Output view in ROV.
SysMin.flushAtExit = false;
*/
/*
* The BIOS module will create the default heap for the system.
* Specify the size of this default heap.
*/
BIOS.heapSize = 0x1000;
/*
* Build a custom SYS/BIOS library from sources.
*/
BIOS.libType = BIOS.LibType_Custom;
/* System stack size (used by ISRs and Swis) */
Program.stack = 0x2000;
/* Circular buffer size for System_printf() */
SysMin.bufSize = 0x200;
/*
* Create and install logger for the whole system
*/
var loggerBufParams = new LoggerBuf.Params();
loggerBufParams.numEntries = 16;
var logger0 = LoggerBuf.create(loggerBufParams);
Defaults.common$.logger = logger0;
Main.common$.diags_INFO = Diags.ALWAYS_ON;
System.SupportProxy = SysMin;
/* ================ Driver configuration ================ */
/* Load the OSAL package */
var osType = "tirtos"
var Osal = xdc.useModule('ti.osal.Settings');
Osal.osType = osType;
/*use CSL package*/
var socType = "am335x";
var Csl = xdc.loadPackage('ti.csl');
Csl.Settings.deviceType = socType;
/* Load the uart package */
var UartPackage = xdc.loadPackage('ti.drv.uart');
UartPackage.Settings.socType = socType;
/* Load the I2C package */
var I2c = xdc.loadPackage('ti.drv.i2c');
I2c.Settings.socType = socType;
/* Load the board package */
var Board = xdc.loadPackage('ti.board');
Board.Settings.boardName = "icev2AM335x";
/* Load Profiling package */
var Utils = xdc.loadPackage('ti.utils.profiling');
/* Load the gpio package */
var GpioPackage = xdc.loadPackage('ti.drv.gpio');
GpioPackage.Settings.enableProfiling = true;
2.3 Build does fail with this output
**** Clean-only build of configuration Debug for project OwnSysBios_TICompiler **** /home/thomas/ti/ccsv7/utils/bin/gmake -j 8 clean -O cleaning ../src/sysbios ... rm -rf "OwnSysBios_TICompiler.hex" "configPkg/linker.cmd" "configPkg/compiler.opt" "OwnSysBios_TICompiler.out" rm -rf "configPkg/" rm -rf "main.obj" rm -rf "main.d" Finished clean **** Build Finished **** **** Build of configuration Debug for project OwnSysBios_TICompiler **** /home/thomas/ti/ccsv7/utils/bin/gmake -j 8 all -O Building file: "../app.cfg" Invoking: XDCtools "/home/thomas/ti/xdctools_3_50_04_43_core/xs" --xdcpath="/home/thomas/ti/bios_6_52_00_12/packages;/home/thomas/ti/pdk_am335x_1_0_10/packages;/home/thomas/ti/uia_2_21_02_07/packages;/home/thomas/ti/ccsv7/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.A8Fnv -p ti.platforms.evmAM3359 -r release -c "/home/thomas/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.6.LTS" --compileOptions "-g --optimize_with_debug" "../app.cfg" making package.mak (because of package.bld) ... generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ... configuring app.xea8fnv from package/cfg/app_pea8fnv.cfg ... generating custom ti.sysbios library makefile ... subdir_rules.mk:10: recipe for target 'build-1140064849-inproc' failed js: "/home/thomas/ti/pdk_am335x_1_0_10/packages/ti/drv/gpio/package.xs", line 115: Error: Library not found: /home/thomas/ti/pdk_am335x_1_0_10/packages/ti/drv/gpio/./lib/a8/release/ti.drv.gpio.profiling.aea8fnv gmake: *** [package/cfg/app_pea8fnv.xdl] Error 1 gmake: *** Deleting file `package/cfg/app_pea8fnv.xdl' gmake: *** [package/cfg/app_pea8fnv.xdl] Deleting file `package/cfg/app_pea8fnv.h' gmake: *** [package/cfg/app_pea8fnv.xdl] Deleting file `package/cfg/app_pea8fnv.c' js: "/home/thomas/ti/xdctools_3_50_04_43_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted. gmake[1]: *** [build-1140064849-inproc] Error 1 gmake: *** No rule to make target 'build-1140064849', needed by 'configPkg/compiler.opt'. Stop. **** Build Finished ****
The problem here is this line: "js: "/home/thomas/ti/pdk_am335x_1_0_10/packages/ti/drv/gpio/package.xs", line 115: Error: Library not found: /home/thomas/ti/pdk_am335x_1_0_10/packages/ti/drv/gpio/./lib/a8/release/ti.drv.gpio.profiling.aea8fnv"
This path does not exist, because of the dot (.) in the path. I investigated why the dot occures there: Within the file "pdk_am335x_1_0_10/packages/ti/drv/gpio/package.xs", the lib path gets modified to ./lib, when the env LIBDIR is not defined:
/* Read LIBDIR variable */
var lib = java.lang.System.getenv("LIBDIR");
/* If NULL, default to "lib" folder */
if (lib == null)
{
lib = "./lib";
} else {
print ("\tSystem environment LIBDIR variable defined : " + lib);
}
I triple checked all the DEFINES and build configurations, between this project and the other PDK-example project which uses GPIO but couldn't make it working.
I also followed the steps of the toolset and glanced into the makefiles to understand why LIBDIR was not set in my case. I gave up since it was to complex to me as a beginner.
With some luck, I tried the same steps with a new CCS-Project template with GNU as toolset. I applied the exact same app.cfg and the build worked!
4. Questions
Now I have a few questions:
4.1 Why does my example not work with TI toolset, but with the GNU ones? I this suppose to be, or a bug?
4.2 Why do I not see the print commands within the .xs-files during the build process? How can I enable this? I already checked
but could not find the answer.
4.3 What is the difference, between TI toolset and the GNU toolset? Which should I use for best stability?
4.4 What is really the minimal configuration to interface GPIO via SysBios? Do I really need UART for this?
4.5 Is there any description, how the build process of SysBios/Drivers/OSAL/CSL works under the hood? My understanding so far (for GPIO as example):
"pdk/packages/ti/drv/gpio/gpio.h" describe a common interface for GPIO functionality, with no dependency on a specific hardware.
The build process picks up the SysBios-configuration and reads the values for the target board and processor, and configures the linker in a way, that it links with the correct hardware implementation.
Is that more or less correct?
Many thanks in advance!