Part Number: AM3352
Customer is having receive sensitivity problems with their AM3552 platform and cellular modem. They tracked down the issue to the VTP calibration causing 6MHz harmonics coming off of the processor. Can VTP calibration be done ONLY at power up or during DDR re-initialization? Wikis seems to indicate this is not a problem.
http://processors.wiki.ti.com/index.php/AM335x_EMIF_Configuration_tips
"VTP_CTRL (@0x44E10E0C) - controls the VTP (Voltage-Temperature-Process) compensation for the DDR I/Os. VTP calibration should occur after the DDR PLL is setup, but before any other DDR controller or DDR PHY configuration is performed. VTP calibration should be performed at power up and each time the DDR controller is re-initialized."
Thanks,
Mark