This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to run encode demo app on dm6446 DVEVM with DVSDK 2.0

HI,

 

I followed step by step instructions given in DVSDK 2.0 GSG. But I am not able to run encode demo application found under dvsdk_demos. Please see the attached file for complete log. 

 

U-Boot 1.3.4 (Jul 30 2010 - 04:43:53)

 

I2C:   ready

DRAM:  256 MB

NAND:  NAND device: Manufacturer ID: 0xec, Chip ID: 0x36 (Samsung NAND 64MiB 1,8V 8-bit)

64 MiB

In:    serial

Out:   serial

Err:   serial

ARM Clock : 297MHz

DDR Clock : 162MHz

Ethernet PHY: LXT972 @ 0x01

Hit any key to stop autoboot:  0 

TFTP from server 10.100.3.241; our IP address is 10.100.3.246

Filename 'uImage'.

Load address: 0x80700000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         ##########

done

Bytes transferred = 2042964 (1f2c54 hex)

## Booting kernel from Legacy Image at 80700000 ...

   Image Name:   Linux-2.6.18_pro500-davinci_evm-

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    2042900 Bytes =  1.9 MB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

 

Starting kernel ...

 

Uncompressing Linux........................................................................................................................................ .

Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (dipen@EICPU1061) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Wed Oct 6 0

CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177

Machine: DaVinci EVM

Memory policy: ECC disabled, Data cache writeback

DaVinci DM6443 variant 0x0

CPU0: D VIVT write-back cache

CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets

CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets

Built 1 zonelists.  Total pages: 30208

Kernel command line: video=davincifb:vid0=0,2500K:vid1=0,2500K:osd0=720x576x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=NTSC daM

PID hash table entries: 512 (order: 9, 2048 bytes)

Clock event device timer0_0 configured with caps set: 07

Console: colour dummy device 80x30

Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)

Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)

Memory: 118MB = 118MB total

Memory: 115200KB available (3493K code, 709K data, 200K init)

Security Framework v1.0.0 initialized

Capability LSM initialized

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

NET: Registered protocol family 16

DaVinci: 71 gpio irqs

WARNING: both IDE and NOR flash are enabled, but share pins.

        Disable IDE for NOR support.

Generic PHY: Registered new driver

ch0 default output "COMPOSITE", mode "NTSC"

MUX: initialized LOEEN

MUX: initialized LFLDEN

VPBE Encoder Initialized

LogicPD encoder initialized

Avnetlcd encoder initialized

SCSI subsystem initialized

usbcore: registered new driver usbfs

usbcore: registered new driver hub

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 4096 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 4096 bind 2048)

TCP reno registered

davinci_spi_board_init: NO spi support

VFS: Disk quotas dquot_6.5.1

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

squashfs: version 3.1 (2006/08/19) Phillip Lougher

JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.

yaffs Oct  6 2010 18:07:00 Installing. 

SGI XFS with no debug enabled

Initializing Cryptographic API

io scheduler noop registered

io scheduler anticipatory registered (default)

LTT : ltt-facilities init

LTT : ltt-facility-core init in kernel

davincifb davincifb: dm_osd0_fb: Initial window configuration is invalid.

davincifb davincifb: dm_osd0_fb: 720x576x16@0,0 with framebuffer size 2025KB

davincifb davincifb: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 2500KB

davincifb davincifb: dm_osd1_fb: 720x480x4@0,0 with framebuffer size 675KB

davincifb davincifb: dm_vid1_fb: 0x0x16@0,0 with framebuffer size 2500KB

davincifb davincifb.0: dm_osd0_fb: Failed to obtain ownership of OSD window.

DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec

Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled

serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A

RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize

Davinci EMAC MII Bus: probed

MAC address is 00:0e:99:02:55:13

TI DaVinci EMAC Linux version updated 4.0

netconsole: not configured, aborting

Linux video capture interface: v2.00

vpfe_init

vpfe_probe

TVP514X : nummber of channels = 1

vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = TVP514X

Trying to register davinci display video device.

layer=c7276a00,layer->video_dev=c7276b60

Trying to register davinci display video device.

layer=c7276800,layer->video_dev=c7276960

davinci_init:DaVinci V4L2 Display Driver V1.0 loaded

i2c /dev entries driver

Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2

ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx

MUX: initialized HDIREN

MUX: initialized ATAEN

    ide0: MMIO-DMA , BIOS settings: hda:pio, hdb:pio

Palm Chip BK3710 IDE Register Fail

Initializing USB Mass Storage driver...

usbcore: registered new driver usb-storage

USB Mass Storage support registered.

usbcore: registered new driver usbhid

drivers/usb/input/hid-core.c: v2.6:USB HID core driver

musb_hdrc: version 6.0, cppi-dma, host, debug=0

musb_hdrc musb_hdrc: No DMA interrupt line

musb_hdrc: USB Host mode controller at c785e000 using DMA, IRQ 12

musb_hdrc musb_hdrc: MUSB HDRC host driver

musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

mice: PS/2 mouse device common for all mice

rtc_davinci_evm rtc_davinci_evm: rtc intf: proc

rtc_davinci_evm rtc_davinci_evm: rtc intf: dev (254:0)

rtc_davinci_evm rtc_davinci_evm: rtc core: registered rtc_davinci_evm as rtc0

rtc0: hours 12-23 are misreported as duplicate hours 00-11

davinci-mmc davinci-mmc.0: Supporting 4-bit mode

davinci-mmc davinci-mmc.0: Using DMA mode

Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).

ASoC version 0.13.1

MUX: initialized MCBSP

AIC3X Audio Codec 0.2

asoc: aic3x <-> davinci-i2s mapping ok

ALSA device list:

  #0: DaVinci EVM (aic3x)

IPv4 over IPv4 tunneling driver

TCP bic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

Time: timer0_1 clocksource has been installed.

Clock event device timer0_0 configured with caps set: 08

Switched to high resolution mode on CPU 0

rtc_davinci_evm rtc_davinci_evm: setting the system clock to 2004-01-01 12:00:11 (1072958411)

applying Intel LTX971 workaround..

Sending DHCP requests .., OK

IP-Config: Got DHCP answer from 192.168.6.59, my address is 10.100.3.246

IP-Config: Complete:

      device=eth0, addr=10.100.3.246, mask=255.255.255.0, gw=10.100.3.1,

     host=10.100.3.246, domain=, nis-domain=(none),

     bootserver=192.168.6.59, rootserver=10.100.3.241, rootpath=

Looking up port of RPC 100003/2 on 10.100.3.241

Looking up port of RPC 100005/1 on 10.100.3.241

VFS: Mounted root (nfs filesystem).

Freeing init memory: 200K

INIT: version 2.86 booting

Starting the hotplug events dispatcher: udevd.

Synthesizing the initial hotplug events...done.

Waiting for /dev to be fully populated...done.

Activating swap...done. 

Remounting root filesystem...done. 

Calculating module dependencies

Loading modules: 

Checking all file systems: fsck

fsck 1.40 (29-Jun-2007)

Mounting local filesystems: mount nothing was mounted

umount.nfs: /dev/root: not found or not mounted

Setting up networking ....

/etc/network/options is deprecated.

Setting up IP spoofing protection: rp_filter done.

Disabling IPv4 packet forwarding: done.

Disabling TCP/IP Explicit Congestion Notification: done.

Starting network interfaces: done.

Starting hotplug subsystem:

   pci     

   pci      [success]

   usb     

   usb      [success]

   isapnp  

   isapnp   [success]

   ide     

   ide      [success]

   input   

   input    [success]

   scsi    

   scsi     [success]

done.

Starting portmap daemon....

Cleaning: /tmp /var/lock /var/run done.

Updating /etc/motd...done.

INIT: Entering runlevel: 3

Starting system log daemon: syslogdNET: Registered protocol family 10

6WIND/LSIIT IPv6 multicast forwarding 0.1 plus PIM-SM/SSM with *BSD API

lo: Disabled Privacy Extensions

IPv6 over IPv4 tunneling driver

Mobile IPv6

 klogd.

Starting NFS common utilities: statd.

Starting internet superserver: inetd.

Starting OpenBSD Secure Shell server: sshd. 

 

MontaVista(R) Linux(R) Professional Edition 5.0.0 (0801921)

 

10.100.3.246 login: root

Last login: Thu Jan  1 12:00:45 2004 on console

Linux 10.100.3.246 2.6.18_pro500-davinci_evm-arm_v5t_le #1 PREEMPT Wed Oct 6 18:12:00 IST 2010 armv5tejl GNU/Linux

 

Welcome to MontaVista(R) Linux(R) Professional Edition 5.0.0 (0801921).

 

root@10.100.3.246:~# cd /opt/dvsdk/dm6446/

root@10.100.3.246:/opt/dvsdk/dm6446# sh loadmodules.sh 

CMEMK module: built on Oct  6 2010 at 18:22:18

  Reference Linux version 2.6.18

  File /opt/TI/dvsdk_2_00_00_22/linuxutils_2_23_01/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c

ioremap_nocache(0x87600000, 10485760)=0xc8000000

allocated heap buffer 0xc8000000 of size 0x2c000

cmem initialized 5 pools between 0x87600000 and 0x88000000

dsplinkk: no version for "struct_module" found: kernel tainted.

DSPLINK Module (1.61.03) created on Date: Oct  6 2010 Time: 18:23:19

root@10.100.3.246:/opt/dvsdk/dm6446# ./encode -v test.mpeg4 

Encode demo started.

ccdc_setstd

ccdc_setstd

Error: Failed to detect video standard, video input connected?

Error: Failed to create video encoder: mpeg4enc

root@10.100.3.246:/opt/dvsdk/dm6446#

 

 

Regards,

Dipen Patel