Part Number: XEVMK2LX
Tool/software: TI-RTOS
I am using the EVMK2LX development board and running the example UART_BasicExample_K2L_c66xExampleProject from the pdk_k2l_4_0_7 folder and I wanted to be able to use UART1 (pins 93,95 on expansion connector). However, I do not see where I can enable UART1. I am also trying to enable SPI2 which also has pins on the expansion connector. It appears that the Board_InitConfig() function is where the program pulls the information regarding what it is using on the board, but I cannot seem to locate the file that it is pulling this data from.
Thank you,
Al