Part Number: AM4376
Hi,
Our customer is considering devices connecting with AM4376 MMC1 or MMC2 interface.
It is used in the following.
· CLK frequency 48MHz
· Voltage 1.8V
The specifications of MMC of AM4376 refer to the following in the datasheet.
Table 5-127. Timing Requirements for MMC [1/2] _ CMD and MMC [1/2] _DAT [7: 0]
Table 5-130. Switching Characteristics for MMC [x] _ CMD and MMC [x] _DAT [7: 0] - HSPE = 1
AM437x Specification
· Delay time td(CLKL-DAT) :(Min) 0.8 ns
· Delay time td(CLKL-CMD) :(Min) 0.8 ns
· Hold time th(CLKH-DATV) :(Min) 2.55 ns
· Hold time th(CLKH-CMDV) :(Min) 2.55 ns
Specification of connected device
· Delay time td(CLKL-DAT) :(Min) 2.5 ns
· Delay time td(CLKL-CMD) :(Min) 2.5 ns
· Hold time th(CLKH-DATV) :(Min) 2.0 ns
· Hold time th(CLKH-CMDV) :(Min) 2.0 ns
Are the above specifications acceptable as specifications of the AM4376 device?
If it is not acceptable, can only be adjusted with external resistance or capcitor?
Please tell me if there is other workaround.
I also see the data sheet of other devices of the TI processor(AM335x,AM57xx etc),
This timing specification is different.
I understand that MMC of AM4376 is created by JEDEC standard.
Is it correct with the recognition that it can be used without problems if it is a device of the JEDEC standard?
Best Regards,
Shigehiro Tsuda