Hello,
I am using OMAP-L138 eXperimenter Kit. Linux 2.6.33-rc4 is running on the ARM side.
I am using the following versions : DaVinci PSP SDK 0.3.20.00.11 and dsplink 1_65_00_02
I successfully rebuilt the linux kernel and uImage. Then i built the DSPLink component using the new uImage built just before.
Then I tried to do the example application using DSP Link on OMAPL1x coming from here :
http://processors.wiki.ti.com/index.php/Example_application_using_DSP_Link_on_OMAPL1x.
I loaded successfully the dsplink module dsplinkk.ko as you can see below, but when i launch the example, i get the following error : PROC_setup () failed. Status = [0x80008008]
***************************************
root@da850-omapl138-evm:/opt/dsplink_test# insmod dsplinkk.ko
DSPLINK Module (1.65.00.02) created on Date: Oct 8 2010 Time: 16:45:15
root@da850-omapl138-evm:/opt/dsplink_test# rm -f /dev/dsplink
root@da850-omapl138-evm:/opt/dsplink_test# mknod /dev/dsplink c 230 0
root@da850-omapl138-evm:/opt/dsplink_test# ./helloDSPgpp helloDSP.out 2
========== Sample Application : helloDSP ==========
Entered helloDSP_Create ()
PROC_setup () failed. Status = [0x80008008]
Leaving helloDSP_Create ()
Entered helloDSP_Delete ()
Assertion failed (IS_VALID_MSGQ (msgqQueue)). File : msgq.c Line : 484
MSGQ_release () failed. Status = [0x8000800b]
Assertion failed (IS_VALID_MSGQ (msgqQueue)). File : msgq.c Line : 335
Leaving helloDSP_Delete ()
====================================================
***************************************
If anybody can help me...
Thanks
Regards
Alex