This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5726: DSP voice libraries support

Part Number: AM5726
Other Parts Discussed in Thread: TMS320C5517

Hi,

I am working on a voice based application where I need VOLIB and AER Libraries to be integrated with, I tested these Libraries on TMS320C5517 fixed point DSP. Now I need to implement the same on Sitara AM572x processor running on Linux. From the release information of these libraries I can find that VOLIB is supported on

 C55x/ C64x+ /C66x processors

and AER is supported on 

28x/55x/62x/64x/64x+/67x/67x+/674x processors

I can also find that Sitara AM572x consist an DSP subsystem with TMS320C66x. Hence even though Sitara AM572x runs on Cortex-A15  core, since it is having C66x as DSP subsystem is it possible to use VOLIB and AER libraries along with Sitara AM572x running on linux?

Expecting a quick response,  Thanks in advance.

Regards,

Janardan M