Part Number: TMS320C6746
Hi, TI!
We have TMS320C6746 in our board. Problem is that some of boards (1-2 per 50 in one production cycle) have issue to crash due to use 2 command of PLL0init in one test programm. When we investigate this problem, it seems that after second command PLL0Init stucks DSP in some state when we cannot write and read data to its internal memory correctly. We use recomendations accordingly page 84 in section 6.6.1 PLL Device-Specific Information and use Murata DLP11SN900HL2L to provide noise immunity. When board power on, voltage on capacitors is 1,34-1,35V. We initialize PLL0init once and voltage drops to 1,29-1,30 that is normal, board working fine like it is supposed. When we initialize PLL0init secondary, voltage rise to 1,321-1,325V and DSP dont write to its memory corretcly. What can cause this problem? Boundary scan diagnostics dont see any problems with this boards, if we use only one PLL0init in program it works fine.