This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMDXEVM8148: Programming bootargs using PCIe u-boot

Part Number: TMDXEVM8148

Tool/software: Linux

Referencing the following documents:

http://processors.wiki.ti.com/index.php/TI81XX_PSP_U-Boot_PCIe_Boot_User_Guide#Components_Involved_in_PCIe_Boot

http://processors.wiki.ti.com/index.php/TI81XX_PSP_UBOOT_User_Guide

The documents mention that:

Bootscript: By default, U-Boot is configured to run a script from location 0x80400000 automatically. This boot script can have commands to set kernel bootargs and load kernel to carry out complete kernel boot automatically. Refer PSP U-Boot user guide for information about writing and creating a U-Boot script using mkimage tool.

All references to the procedures assume a command prompt and a TFTP connection.  PCIe u-boot does  not have either.

How does the boot script get programed into memory at 0x80400000 when there is no command prompt?

Is there a method to modify a default boot script that the PCIe u-boot will use when booting Linux?

Steve

  • Hi,

    Support for this device is very limited, for any detailed software or hardware support, bug fixes, or enhancements to the software, please contact the partners recommended below. They have extensive software expertise and systems experience. Customers starting new designs are also recommended to contact these ecosystem partners for prepackaged hardware and software solutions, as well as for full design consultation and support.

    Path Partner Technology (sales@pathpartnertech.com)

    Regards,
    Bhavin Kharadi