I'm trying to determine the latency of this encoder. I don't understand how to translate the performance statistic numbers in Table 2 and the Encoding Times in Figure 1 to a latency number in seconds per frame. Why is Performance Statistic Table 2 in Megacycle per second? How do I calculate the encoder latency using the Performance Statistic?
I use Figure 1, the max encodint time is about 25 megacycles. Would that mean the max latency is 25 x 10e6 / 594 x 10e6 = 42.1 msec?? Doesn't that exceed the 33.33 msec frame period at 30 fps?? It doesn't make sense.