This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5718: Boot issue at high temperatures

Part Number: AM5718

Tool/software: Linux

Dear team,

I am using am5718.

I found crypto module and some firmware can not be loaded well under high temperature environment when booting linux .

error log:

[   11.698042] omap_sham_cra_init_alg: omap-sham: fallback driver 'sha512' could not be loaded.
[   11.852430] omap_sham_cra_init_alg: omap-sham: fallback driver 'md5' could not be loaded.
[   11.860661] omap_sham_cra_init_alg: omap-sham: fallback driver 'sha1' could not be loaded.
[   11.939830] omap_sham_cra_init_alg: omap-sham: fallback driver 'sha224' could not be loaded.
[   11.980216] omap_sham_cra_init_alg: omap-sham: fallback driver 'sha256' could not be loaded.
[   12.077585] omap_sham_cra_init_alg: omap-sham: fallback driver 'sha384' could not be loaded.
[   12.077598] omap_sham_cra_init_alg: omap-sham: fallback driver 'sha512' could not be loaded.

[   69.600939] vpe 489d0000.vpe: couldn't get firmware
[   69.605869] remoteproc remoteproc2: powering up 40800000.dsp
[   69.611697] remoteproc remoteproc1: powering up 55020000.ipu
[   69.611707] ------------[ cut here ]------------
[   69.611720] WARNING: CPU: 0 PID: 84 at drivers/base/firmware_class.c:1166 _request_firmware+0x318/0x6f0
[   69.611838] Modules linked in: bc_example(O) xhci_plat_hcd pru_rproc xhci_hcd pruss_intc usbcore pruss dwc3 udc_core usb_common snd_soc_simple_card snd_soc_simple_card_utils xfrm_user pwm_fan xfrm4_tunnel ipcomp xfrm_ipcomp esp4 ah4 snd_soc_omap_hdmi_audio af_key xfrm_algo pvrsrvkm(O) omap_aes_driver c_can_platform ahci_platform c_can libahci_platform libahci pruss_soc_bus omap_sham can_dev omap_wdt libata scsi_mod ti_vip ti_vpe ti_vpdma ti_sc ti_csc dwc3_omap extcon_core ti_cal gpio_pisosr omap_hdq wire gt911 rtc_rx8010 ov5640_mipi omap_des ov5640 snd_soc_wm8960 des_generic crypto_engine omap_remoteproc virtio_rpmsg_bus rpmsg_core remoteproc uio_module_drv(O) uio gdbserverproxy(O) cryptodev(O) cmemk(O)
[   69.611846] CPU: 0 PID: 84 Comm: kworker/0:3 Tainted: G           O    4.9.41-ga8674b1 #392
[   69.611849] Hardware name: Generic DRA72X (Flattened Device Tree)
[   69.611859] Workqueue: events request_firmware_work_func
[   69.611863] Backtrace:
[   69.611875] [<c020b29c>] (dump_backtrace) from [<c020b558>] (show_stack+0x18/0x1c)
[   69.611882]  r7:00000009 r6:600c0013 r5:00000000 r4:c10229d0
[   69.611891] [<c020b540>] (show_stack) from [<c04acda0>] (dump_stack+0x8c/0xa0)
[   69.611899] [<c04acd14>] (dump_stack) from [<c022e3e8>] (__warn+0xec/0x104)
[   69.611905]  r7:00000009 r6:c0bee1cc r5:00000000 r4:00000000
[   69.611912] [<c022e2fc>] (__warn) from [<c022e4b8>] (warn_slowpath_null+0x28/0x30)
[   69.611919]  r9:df7fa8c0 r8:df7fa5c0 r7:df7fa8c0 r6:eebc5e5c r5:fffffff5 r4:ee1a1440
[   69.611926] [<c022e490>] (warn_slowpath_null) from [<c0619d38>] (_request_firmware+0x318/0x6f0)
[   69.611933] [<c0619a20>] (_request_firmware) from [<c061a158>] (request_firmware+0x48/0x60)
[   69.611940]  r10:eeb9cf80 r9:00000000 r8:ee139c20 r7:ee139c20 r6:ee1a1440 r5:eebc5e5c
[   69.611942]  r4:00000000
[   69.611967] [<c061a110>] (request_firmware) from [<bf030bd4>] (__rproc_boot+0xec/0x5bc [remoteproc])
[   69.611972]  r7:00000000 r6:ee139dcc r5:ee139dc4 r4:ee139c00
[   69.612000] [<bf030ae8>] (__rproc_boot [remoteproc]) from [<bf0310d0>] (rproc_auto_boot_callback+0x18/0x24 [remoteproc])
[   69.612006]  r10:eeb9cf80 r9:00000000 r8:ef64cd00 r7:00000000 r6:ef649600 r5:eeb9cf80
[   69.612009]  r4:00000000
[   69.612026] [<bf0310b8>] (rproc_auto_boot_callback [remoteproc]) from [<c061a300>] (request_firmware_work_func+0x44/0x6c)
[   69.612030]  r5:eeb9cf80 r4:ee1a1c80
[   69.612038] [<c061a2bc>] (request_firmware_work_func) from [<c0244d84>] (process_one_work+0x1dc/0x3f8)
[   69.612040]  r4:ee1a1c80
[   69.612047] [<c0244ba8>] (process_one_work) from [<c02459dc>] (worker_thread+0x58/0x574)
[   69.612052]  r10:eeb9cf80 r9:eebc4000 r8:ef649618 r7:c1002d00 r6:00000008 r5:eeb9cf98
[   69.612055]  r4:ef649600
[   69.612063] [<c0245984>] (worker_thread) from [<c024ad14>] (kthread+0x100/0x118)
[   69.612068]  r10:00000000 r9:00000000 r8:c0245984 r7:eeb9cf80 r6:eebc4000 r5:eeb99fc0
[   69.612070]  r4:00000000
[   69.612079] [<c024ac14>] (kthread) from [<c0207c88>] (ret_from_fork+0x14/0x2c)
[   69.612084]  r8:00000000 r7:00000000 r6:00000000 r5:c024ac14 r4:eeb99fc0
[   69.612087] ---[ end trace ae9e842ece03b5a9 ]---
[   69.612092] remoteproc remoteproc1: firmware: dra7-ipu2-fw.xem4 will not be loaded
[   69.612099] remoteproc remoteproc1: request_firmware failed: -11
[   69.612119] remoteproc remoteproc0: powering up 58820000.ipu

some thermal info is below, if beyond this, the error will happen when linux bootting:

cpu_thermal
68600
gpu_thermal
69400
core_thermal
68600
dspeve_thermal
67800
iva_thermal
68600
board_thermal
53875

------------------------------------------------------------------------------------------------------------------------

------------------------------------------------------------------------------------------------------------------------

when the termal info below this, the linux can boot without error。

cpu_thermal
65400
gpu_thermal
66600
core_thermal
65400
dspeve_thermal
65800
iva_thermal
66200
board_thermal
50812

how to solve the problem?