Tool/software: Code Composer Studio
Hi,
I’m trying to run NDK example on C66x core but it doesn’t work.
In “Running NDK Examples for KeyStone™ Devices” of the documentation, the step 4 is : Run the setupPhy script (Scripts → DSP Clock Estimation → setupPhy). However “setupPhy” is not available in the menu.
I use this GEL File : ~\ccs_v7.3\ccsv7\ccs_base\emulation\boards\xtcievmk2x\gel\xtcievmk2x.gel
Also to compile the project, I need to specify these arguments in “Predefined Symbols” (-D) : SOC_K2H and DEVICE_K2H.
I’m running the example only on core0.
When I run the program, I get this output :
[C66xx_0] QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
TCP/IP Stack 'Hello World!' Application
StackTest: using localIp
I try with static IP and DHCP (no DHCP request on the network)
Version :
CCS : 7.3.0
NDK : 2.26.00.08
Bios : 6.52.00.12
Pdk k2hk : 4.0.8
Thanks,
Leo