This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ramdisk Test on DM6467

Other Parts Discussed in Thread: ASH

Hi,

 

I wanna make a RamDisk for DM6467. I followed the instructions at http://processors.wiki.ti.com/index.php/How_to_Create_a_Ramdisk_with_Auto-run_Demo.

I cannot run /etc/rc.d/rc.local .

 

By NFS, rc.local runs automatically after booting.

When put in Ramdisk, it failed to run automatically.

Please see the log below.

========================================================================

Starting hotplug subsystem:
   pci
   pci      [success]
   usb
   usb      [success]
   isapnp
   isapnp   [success]
   ide
   ide      [success]
   input
   input    [success]
   scsi
   scsi     [success]
done.
Starting portmap daemon: portmap/etc/rc.d/rcS.d/S41portmap: 156: nice: not found

pidof: invalid option -- x
BusyBox v1.01 (2005.12.18-04:57+0000) multi-call binary

No help available.

.
/etc/init.d/rcS: 60: /etc/rc.d/rc.local: not found
INIT: /Entering runlevel: 3
Starting internet superserver: inetd.

========================================================================


I checked the files on RamDisk

The rc.local exists.

# cd etc
cd: 1: can't cd to etc
# cd /etc/rc.d
# ls
1;36minit.d0m    1;34mrc0.d0m     1;34mrc2.d0m     1;34mrc4.d0m     1;34mrc6.d0m

1;32mrc.local0m  1;34mrc1.d0m     1;34mrc3.d0m     1;34mrc5.d0m     1;34mrcS.d0m

# ls -l
lrwxrwxrwx    1 root     root            9 Oct 10  2010 1;36minit.d0m -> 1;34m..
/init.d0m
-rwxrwxrwx    1 root     root           43 Oct  9  2010 1;32mrc.local0m
drwxr-xr-x    2 root     root         1024 Dec 29  2005 1;34mrc0.d0m
drwxr-xr-x    2 root     root         1024 Dec 29  2005 1;34mrc1.d0m
drwxr-xr-x    2 root     root         1024 Dec 29  2005 1;34mrc2.d0m
drwxr-xr-x    2 root     root         1024 Dec 29  2005 1;34mrc3.d0m
drwxr-xr-x    2 root     root         1024 Dec 29  2005 1;34mrc4.d0m
drwxr-xr-x    2 root     root         1024 Dec 29  2005 1;34mrc5.d0m
drwxr-xr-x    2 root     root         1024 Dec 29  2005 1;34mrc6.d0m
drwxr-xr-x    2 root     root         1024 Dec 29  2005 1;34mrcS.d0m
#

What's the reason?

 

thanks.