Hi,
We are planning to use OMAP3503 with eMMC for boot and storage in our design. We are using eMMC [Part No: THGBM1G4D1EBAI7] from Toshiba.
Can you please provide us the following information.
1. Can we use any MMC1 or MMC2 port of OMAP35x for eMMC boot? or any restriction (like Power sequence, IO Voltage etc..)?
2. Is Boot ROM supports 8-bit Mode or only 1-bit mode? If only 1-bit mode what is the max performance (MBps)?
3. What is the Maximum performance (MBps) achieved in 8-bit mode/4-bit mode?
Looking forward you support.
Thanks
Ranjith