Other Parts Discussed in Thread: TPS65930, OMAP3530, TPS65950
Hi ,
In our OMAP35x based design, we are using TPS65930 PMIC for Power supply.
We are using MMC PORT-1 from OMAP for eMMC interface and eMMC is used for booting. The IO logic is 3.0v.
We have connected VDDS_MMC1 of OMAP to VMMC1_LDO of PMIC.
As per the PMIC datasheet, VMMC1_LDO output is OFF in default.
The OMAP ROM code configures the PMIC through I2C to set VMMC1_LDO is set to 3.0 V when booting from MMC port 1 is requested from the sys-boot pins.
In TPS65930 PMIC datasheet [SWCS037E, Page 28/114, Table 4-1], the default voltage VMMC1_LDO mentioned as 1.8V
But as per User Manual Ver D [Page 401/800] mentioned as
“The default output voltage of VMMC1 for the Master_C027 boot mode is 1.85 V, which corresponds to a value of 0x0 for the VSEL bit field “
It looks contradictory. Please confirm, what is the default output voltage of VMMC1_LDO of TPS65930 PMIC?
Is the MMC (or eMMC) OMAP boot tested with TPS65930 PMIC?
Thanks
Ranjith