Part Number: PROCESSOR-SDK-C665X
Hello!
I think the Keystone supports maximum 8 Gigabyte RAM, is that right?
The 8 Gigabit DDR3 chip from Micron MT41K512M16HA-125 IT:A has 8Gbit = 1 Gigabyte RAM and is 16 Bits wide. 4 pieces of this device result in only 4 Gigabyte total
An alternative part with similar specification is the Intelligent Memory 8 Gigabit 1CS part# IM8G16D3FCBG-125I
a) Would it also be possible to use 8 pieces of 8 Gigabit with a 8 bit wide interface like IM8G08D3FCBG-125I or MT41K1G8SN-125 IT:A ?
b) Does the Keystone support a second chip-select (CS), clock enable (CKE), ODT and ZQ to add a second rank of another 4 pieces of 16 Bit wide components with 8 Gigabit each?
c) If the answer to b) is yes, can I assume that it will also be possible to use 4 pieces of a future 16 Gigabit DDR3 component with two sets of CS, CKE, ODT and ZQ pins? Intelligent Memory is planning to release such a device with dual-CS later this year. This would allow to reach total 8 Gigabyte of memory by only 4 pieces of DDR3 components!
Regards,
Thorsten