Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AM5728: McASP usage from DSP

Part Number: AM5728

Tool/software: TI-RTOS

Hi,

 

I am working on custom board using AM5728 with Linux on A15 and TI RTOS on DSP1. I am trying to setup MCASP5 for TX on AXR0 in 32-bit I2S mode for 2 slots. I have initialized EDMA, configured XBAR. I have configured ACLKX = 1.026MHz, FSX = 15.9KHz. The external reference clock is 24.576MHz. I verified ACLKX and FSX being output using scope.

FYI, the Mcasp_HwSetupData used is -

   { /* MCASP5_TX */

           0xFFFFFFFF,   // MCASP_TXMASK

           0x000180F0,   // MCASP_TXFMT

           0x00000113,   // MCASP_TXFMCTL

           0x00000003,   // MCASP_TXTDM

           0x0000000F,   // MCASP_EVTCTLX

           0x000001FF,   // MCASP_TXSTAT

           0x00000000,   // MCASP_XEVTCTL

           {

                   0x00000022, // MCASP_ACLKXCTL

                   0x00008098, // MCASP_AHCLKXCTL

                   0x00000000 // MCASP_TXCLKCHK

          }

   }

 

And Mcasp_ChanParams are –

 

   { /* MCASP5_TX */

           1,

           { Mcasp_SerializerNum_0 },

           &mcasp_setup[MCASP5_TX], // as above

           TRUE,

           Mcasp_OpMode_TDM,

           Mcasp_WordLength_32,

           NULL,

           0,

           NULL,

           (Mcasp_GblCallback)M5_GblErrXmt,

           2,

           Mcasp_BufferFormat_1SER_MULTISLOT_INTERLEAVED,

           TRUE,

           4, // 2

           TRUE

   }

 

In my code, I am getting callbacks for each MCASP transactions submitted using mcaspSubmitChan(). I have 2 transmit buffers (PING, PONG) with 5ms length. (Buffers are allocated memory using Memory_calloc() and aligned by 128). In the callback, I am checking for under run by means of counting semaphore posts. In the task loop, I am waiting on semaphore, loading data into the transmit buffer and calling CacheP_wbInv() before submitting the loaded transmit buffer using mcaspSubmitChan().

 

On the scope, I don’t see the data I load into TX buffer being sent out from the AXR0 – it’s all 0s except the 0x0080_0000 being sent out every 10ms (i.e. 2x audio frame size). What am I missing? I have tried re-building pdk with Mcasp_LOOPJOB_ENABLED feature disabled and that didn't help.

(I am using RTOS and Linux SDK v4.01 with CCSv7.2)