This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TDA2: Files needed for running SemSeg Semantic Segmentation usecase (Vision SDK, tidl)

Part Number: TDA2

Tool/software: TI-RTOS

Hi,

We have a TDA2X dev board and using Vision SDK 3.2.0.0

If I understand it correctly, we need additional files (besides the code in AppImage) to run this example:

1) Input video and header files. At this point we would love to have sample files, but I do not have access to CDDS yet. 
Is there a specific requirements for video format, resolution required, etc?
I saw some info and even sample files 700x400 in another thread here, but now sure if this video works or not. I can try.

2) Since SemSeg uses TIDL, we probably need the right converted model files like NET.BIN, PRM.BIN, etc ? Right? Where can I find them?
There are some example files in vision_sdk\apps\tools\TIDL_files folder, but I do not think these are the right ones for SemSeg usecase...

Thanks,

Mikhail