This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interrupt on TMS320VC5505-eZDSp

Hi,

I have spent almost 3-4 weeks to get properly init the timer0 interrupt, 

The interrupt examples,user guides given by TI is create more confusion and also it eat our time.

 

The attached example code is simple, in this example the Timer-0 is initialized to interrupt the CPU at every "21.1micro sec"

setting GPIO as INPUT or OUTPUT (both option is available)

just wanted to give SOME guidance so others don't have to spend the hours and hours it took me find all these pesky details.

 

 

Ashwin Panchal