Part Number: TMS320DM8148
Hello,
We are building application with codesourcesey 2009q1-203 with dm8148,
It seems to all work fine.
But we need to add GDB debugger in windows.
Trying to use the gdbserver from the codesourcesey toolchain we get the following error in gdb host:
Error in final launch sequence
Failed to execute MI command:
-file-exec-and-symbols Debug/simple_hello
Error message from debugger back end:
Dwarf Error: wrong version in compilation unit header (is 4, should be 2) [in module c:\users\ransh\workspace_v7\simple_hello\debug\simple_hello]
Dwarf Error: wrong version in compilation unit header (is 4, should be 2) [in module c:\users\ransh\workspace_v7\simple_hello\debug\simple_hello]
Thank you for any advise,
ran