Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
Hello,
I am interfacing a codec (master) with a fixed 256 x fs bclk ratio regardless of slots or slot width to the McASP (slave).
I would prefer to do this with simple-card instead of implementing a separate machine driver just to make this one setting.
I have studied the device tree bindings of both the simple-card and McASP and I don't see anything that would make this setting explicitly.
I have also taken a look at the source of the McASP platform driver and it isn't immediately obvious how this would happen other than using set_clkdiv call back which the simple-card does not use.
I thought there may be a way to do this implicitly. For example, I have tried to set 8 slots and 32 slot width with the set_tdm_slot callback.
I am hoping there are some experts here who can tell be if it is possible to use simple-card to interface the codec I have to the McASP.
Regards,
Steven