This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM57X: 4K encode support

Part Number: PROCESSOR-SDK-AM57X


The release notes of PSDK 4.03 highlights a new demo addition (Demonstrate 4K Video Encode with IVAHD on AM57x).

I realize this is a file to file 4K encoding demo. I would like to know the following info regarding 4k support in the PSDK

  1. Is the support only to demostrate the H.264 codec capabilities for 4K encode?
  2. Are there any changes/enhancements to VIP or vpe or display or other components to support 4K?
  3. Is it possible to realize a 4k streaming (capture-Encode-Stream) gstreamer pipeline using this PSDK?
  4. Does IVAHD decoder has support for 4K decode? If yes, is it possible to realize a 4k decode (Receive-Decode-Display) pipeline?