Hello,
Can you support with a customer query;
1. Could you confirm that this device is capable of operating as a Profinet Master(with or without the correct software stack)?
2. We are keen to modify this device according to our requirements – I have located the schematic .pdf and .DSN files, but would like to be able to modify them in our schematic capture and layout tool – DxDesigner, (or alternatively Eagle). Please could you send us editable versions? Or are these unavailable due to intellectual property?
the question is related to; Certified Profinet IRT V2.3 Device with 1 GHz ARM Application Processor Reference Design
Will appreciate the help.
BR
Linda