This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Do I use another OS except Montavisa in the DM6446?

Hi,

Do I use another OS except Montavisa in the DM6446? The kernel more than >2.6.10.

If it can, how can install the DSP?

Thanks.

  • I meaning embedded linux.

  • DM6446 contains two CPU cores, and ARM9 and a DSP.  On the DSP, you typically run DSP/BIOS operating system, on ARM side, you can run Linux, WinCE, Integrity...and other operating systems.  If you want to stick with Linux, our latest official release is based on 2.6.10 kernel.

    There is an early adoptor release of the DM6446 linux kernel based on 2.6.18, but I would not recommend using it unless you really need to.  You can avoid yourself many headaches by waiting for the official dvsdk 2.0 release which will include this kernel.  If you still want to give it a go, here is the link: https://www-a.ti.com/downloads/sds_support/targetcontent/dvsdk/mv_dvsdk/v2_00/index_external.html

  • I'm using the 2.6.18_pro500-davinci_ev-arm_v5t_le kernel provided by mvl_5_0_0_demo_lsp_setuplinux_02_10_00_18.bin with a hand made armv5tel-softfloat-linux-gnueabi toolchian (via the 'crossdev' tool of Gentoo, `crossdev -t armv5tel-softfloat-linux-gnueabi`).

    the versions of the toolchain are...

    • binutils-2.19.1-r1
    • linux-headers-2.6.28-r1
    • glibc-2.9_p20081201-r2
    • gcc-4.3.3-r2

    and a corresponding handmade Gentoo armv5tel distro.

    The kernel itself compiles and boots without any problem, so does the userspace distro. Everything works well, such as USB, ALSA, fbdev, and other peripherals. And the most important thing is, performance is a *LOT* more better than montavista linux 4.0 + gcc 3.4.

    But, I just can never get dsplink to work. it either says memory map configuration mismatch, or kernel panic, or crash without any message. I've tried several combinations of codec engine, dsplink, codegen tools, and xdctools, without success.

    versions and combinations i've used:

    • dvsdk_setuplinux_1_30_01_41.bin
    • dvsdk_setuplinux_2_00_00_18.bin
    • TI-C6000-CGT-v6.0.22.bin
    • TI-C6000-CGT-v6.1.9.bin
    • xdc_setuplinux_3_00_02_14.bin
    • xdctools_setuplinux_3_10_01.bin
    • xdctools_setuplinux_3_15_00_50.bin
    • dsp_bios_setuplinux_5_31_81_15.bin
    • bios_setuplinux_5_33_04.bin
    • codec_engine_1_20_03.tar.gz
    • codec_engine_2_10_02.tar.gz
    • codec_engine_2_21 (privided by dvsdk_2_00_00_18)
    • codec_engine_2_23_01.tar.gz
    • dsplink_1_40_05_p4.tar.gz (I did this by untar p1 p2 p3 p4 over an 1_40_05 directory, and applied a patch from http://www.mail-archive.com/davinci-linux-open-source@linux.davincidsp.com/msg09930.html to make it compiles against kernel-2.6.18)
    • dsplink_1_51.tar.gz
    • dsplink_1_60.tar.gz
    • dsplink-1_60-prebuilt (provided by dvsdk_2_00_00_18)
    • dsplink_1_61_03.tar.gz
    • linuxutils_2_22_01 (provided by dvsdk_2_00_00_18)
    • linuxutils_2_23_01.tar.gz

    When I use the provided stack inside dvsdk_2_00_00_18 + C6000-CGT-<whatever version> + xdctools_<whatever version>, the decode demo hang at
    @2,234,106us: [+0 T:0x4140d490 S:0x4140ca14] OC - Comm_create> return (0x9d098)
    @2,234,364us: [+0 T:0x4140d490 S:0x4140ca1c] OC - Comm_put> Enter(queue=0x0, msg=0x41c11c80)
    @2,234,686us: [+0 T:0x4001fd10 S:0xbed1afdc] OC - Comm_put> Enter(queue=0x0, msg=0x41c12c80)

    When i switch dsplink to 1.61.03, it first complains about gpp and dsp version mismatch. So I `mv decodeCombo_e.x64P decodeCombo.x64P` and it runs, but always complain about a configuration mismatch. I've checked everywhere for those DSPALGHEAP, DDR2, DSPLINKMEM, RESET_VECTOR but can never get things right.

    With dsplink 1.40.05-p4, kernel oops. the stack backtrace follows:
    [  420.720000] Backtrace:
    [  420.720000] [<bf0df388>] (LDRV_freeLinkCfg+0x0/0x40c [dsplinkk]) from [<bf0e014c>] (LDRV_getLinkCfg+0x9b8/0x9e8 [dsplinkk])
    [  420.720000]  r6 = 0363E1D0  r5 = C7866000  r4 = 80008008
    [  420.720000] [<bf0df794>] (LDRV_getLinkCfg+0x0/0x9e8 [dsplinkk]) from [<bf0df280>] (LDRV_init+0x34/0x13c [dsplinkk])
    [  420.720000] [<bf0df24c>] (LDRV_init+0x0/0x13c [dsplinkk]) from [<bf0d3260>] (PMGR_PROC_setup+0xa4/0x128 [dsplinkk])
    [  420.720000]  r4 = 00008000
    [  420.720000] [<bf0d31bc>] (PMGR_PROC_setup+0x0/0x128 [dsplinkk]) from [<bf0d04a4>] (DRV_Ioctl+0x41c/0xcc4 [dsplinkk])
    [  420.720000]  r7 = 40BDFD68  r6 = 00006C01  r5 = C323DEE4  r4 = 00006C01
    [  420.720000] [<bf0d0088>] (DRV_Ioctl+0x0/0xcc4 [dsplinkk]) from [<c00fd814>] (do_ioctl+0x7c/0x98)
    [  420.720000]  r8 = 00000006  r7 = 40BDFD68  r6 = 00006C01  r5 = 40BDFD68
    [  420.720000]  r4 = C4B6E220
    [  420.720000] [<c00fd798>] (do_ioctl+0x0/0x98) from [<c00fdaf0>] (vfs_ioctl+0x2c0/0x2ec)
    [  420.720000]  r6 = 00006C01  r5 = C4B6E220  r4 = 00000006
    [  420.720000] [<c00fd830>] (vfs_ioctl+0x0/0x2ec) from [<c00fdbd0>] (sys_ioctl+0xb4/0xe8)
    [  420.720000]  r7 = C4B6E220  r6 = 00006C01  r5 = 40BDFD68  r4 = 00000000
    [  420.720000] [<c00fdb1c>] (sys_ioctl+0x0/0xe8) from [<c0088ff8>] (__sys_trace_return+0x0/0x28)
    [  420.720000]  r8 = C0089028  r7 = 00000036  r6 = 0009CDD8  r5 = 00062CBC
    [  420.720000]  r4 = 00000000
    [  420.720000] Code: ea00001a e590300c e590202c e0833006 (e5930038)

    My questions:

    • Is there an "Changing the DVEVM Memroy Map" article that applies to dsplink-1.60+ and ce-2.23+? If so, where is it?
    • How do i build the l64P files inside dm6446_dvsdk_combo_2_03 directories? The provided production l64P's are all 0kb in size, and when I issue `make XDCARGS=prod` it always tell me "File not recognized."

    thanks!

  • Did you install all the software from https://www-a.ti.com/downloads/sds_support/targetcontent/dvsdk/mv_dvsdk/v2_00/index_external.html (link I previously sent)?

    According to the DM6446 release notes available from the link above, you should be using dsplink 1.60; I would use the pre-built ones for now.

    Palatis said:

    My questions:

    • Is there an "Changing the DVEVM Memroy Map" article that applies to dsplink-1.60+ and ce-2.23+? If so, where is it?
    • How do i build the l64P files inside dm6446_dvsdk_combo_2_03 directories? The provided production l64P's are all 0kb in size, and when I issue `make XDCARGS=prod` it always tell me "File not recognized."

    Yes the memory map article applies to this versions as well; as you will see in the article, there is a separate section for the different versions of dsplink.

    The codec libraries (l64P) files are not included in the DVSDK; you will need to request them via http://focus.ti.com/dsp/docs/dspfindtoolswbytooltype.tsp?sectionId=3&tabId=1460&toolTypeId=65&familyId=44

     

  • Even if I use all pre-built ones (kernel, cmemk.ko, dsplinkk.ko, mvl demo target sys (nfs mounted), decode executable, and the decodeCombo.x64P), I still get kernel panic.

    Unable to handle kernel NULL pointer dereference at virtual address 00000000
    pgd = c0004000
    [00000000] *pgd=00000000
    Internal error: Oops: 17 [#1]
    Modules linked in: dsplinkk cmemk
    CPU: 0
    PC is at __wake_up_common+0x18/0x78
    LR is at __wake_up+0x40/0x80
    pc : [<c0040428>]    lr : [<c0041d0c>]    Tainted: GF   
    sp : c07f5e10  ip : 00000000  fp : c07f5e3c
    r10: 00000000  r9 : c07f5e60  r8 : c03d65b8
    r7 : 00000000  r6 : c002c360  r5 : c61425c0  r4 : 00000013
    r3 : 00000001  r2 : 00000001  r1 : 00000006  r0 : c0000000
    Flags: nzcv  IRQs off  FIQs on  Mode SVC_32  Segment kernel
    Control: 5317F
    Table: 80EA8000  DAC: 00000017
    Process rpciod/0 (pid: 187, stack limit = 0xc07f4258)
    Stack: (0xc07f5e10 to 0xc07f6000)
    5e00:                                     c0059254 00000013 c61425c0 c002c360
    5e20: 00000000 c03d65b8 c02ce7b4 00000000 c07f5e5c c07f5e40 c0041d0c c0040420
    5e40: c07f5e60 016a0d5f c07f5e7c c049a1c0 c07f5e74 c07f5e60 c005cf7c c0041cdc
    5e60: c049a1c0 00000000 c07f5e8c c07f5e78 c006f96c c005cf58 c010fcc0 c6142460
    5e80: c07f5ebc c07f5e90 c0111504 c006f934 c07f5ebc c6142460 c6142464 c61424cc
    5ea0: 00000000 c6142460 c61425c0 00000000 c07f5edc c07f5ec0 c0112054 c01114f8
    5ec0: c02c905c c6142464 00000000 c61424cc c07f5ef4 c07f5ee0 c02ce7e8 c0111f44
    5ee0: 00000000 c6142464 c07f5f24 c07f5ef8 c02ce1d0 c02ce7c4 c71ed2d4 80000013
    5f00: c07d1f20 c07f4000 c61424d4 00000000 c02ce364 c6142464 c07f5f34 c07f5f28
    5f20: c02ce374 c02ce134 c07f5f6c c07f5f38 c0059698 c02ce374 c07d1f38 c07d1f28
    5f40: 00000002 00000000 c07d1f28 c07f4000 c07d1f20 c07d1f30 00000002 c07f5f84
    5f60: c07f5fcc c07f5f70 c0059ea0 c00595c8 00000001 00000000 00000000 00010000
    5f80: 00000000 00000000 c7194c20 c0041a98 00100100 00200200 ffffffff ffffffff
    5fa0: 00000000 c07d1f20 c07f4000 c0059d98 c050fb58 00000000 00000000 00000000
    5fc0: c07f5ff4 c07f5fd0 c005ce8c c0059da8 ffffffff ffffffff 00000000 00000000
    5fe0: 00000000 00000000 00000000 c07f5ff8 c0049810 c005cdb4 421f08f4 7b2196c1
    Backtrace:
    [<c0040410>] (__wake_up_common+0x0/0x78) from [<c0041d0c>] (__wake_up+0x40/0x80)
    [<c0041ccc>] (__wake_up+0x0/0x80) from [<c005cf7c>] (__wake_up_bit+0x34/0x3c)
     r4 = C049A1C0
    [<c005cf48>] (__wake_up_bit+0x0/0x3c) from [<c006f96c>] (unlock_page+0x48/0x4c)
    [<c006f924>] (unlock_page+0x0/0x4c) from [<c0111504>] (nfs_readpage_release+0x1c/0x98)
     r4 = C6142460
    [<c01114e8>] (nfs_readpage_release+0x0/0x98) from [<c0112054>] (nfs_readpage_result_full+0x120/0x144)
     r6 = 00000000  r5 = C61425C0  r4 = C6142460
    [<c0111f34>] (nfs_readpage_result_full+0x0/0x144) from [<c02ce7e8>] (rpc_exit_task+0x34/0x74)
     r6 = C61424CC  r5 = 00000000  r4 = C6142464
    [<c02ce7b4>] (rpc_exit_task+0x0/0x74) from [<c02ce1d0>] (__rpc_execute+0xac/0x240)
     r4 = C6142464
    [<c02ce124>] (__rpc_execute+0x0/0x240) from [<c02ce374>] (rpc_async_schedule+0x10/0x14)
    [<c02ce364>] (rpc_async_schedule+0x0/0x14) from [<c0059698>] (run_workqueue+0xe0/0x170)
    [<c00595b8>] (run_workqueue+0x0/0x170) from [<c0059ea0>] (worker_thread+0x108/0x144)
    [<c0059d98>] (worker_thread+0x0/0x144) from [<c005ce8c>] (kthread+0xe8/0x128)
    [<c005cda4>] (kthread+0x0/0x128) from [<c0049810>] (do_exit+0x0/0xa24)
     r7 = 00000000  r6 = 00000000  r5 = 00000000  r4 = 00000000
    Code: e24cb004 e24dd004 e590c000 e59b9004 (e59c5000)
     <6>note: rpciod/0[187] exited with preempt_count 1

  • Juan Gonzales said:

    There is an early adoptor release of the DM6446 linux kernel based on 2.6.18, but I would not recommend using it unless you really need to.  You can avoid yourself many headaches by waiting for the official dvsdk 2.0 release which will include this kernel.

    Hi Juan, do you have any suggestions about the date of the official dvsdk 2.0 release?

    I ask, because we are just starting a new DM6467 project and want to find out if it's better to take MV4.0.1 with DVSDK 1.40.xx.xx, which is quite old but expected to be stable and widely used, or if it's worth to wait for dvsdk 2.0. - I presume, dvsdk 2.0 is required, if I want to use MV 5.0, correct?

    Thanks, Malte

  • you are correct that DVSDK 2.0 is required if you want MV pro 5.0.  I do not believe it should be much longer for DVSDK 2.0 to come out, but let me do a little digging before posting a time frame. 

    I always tend to recommend the stable DVSDKs (less head-aches like the dpslink stuff you are running into), but since you thought the EA DVSDK 2.0 was much better, and I do not expect a big delay for this to come out, you may want to stick with this one.  Can you make other progress while we look at the dsplink stuff.  I was planning on trying to run the demo later on today.

  • Where exactly do I confirm ARM(GPP) side and DSP side memory map configurations?

    I double checked the following files:

    • dsplink_1_61_03/packages/dsplink/
      • config/all/CFG_DM6446GEM_SHMEM.c
      • config/BUILD/CFG_DM6446GEM_SHMEM.c
      • dsp/inc/DspBios/5.XX/DM6446GEM/dsplink-dm6446gem-base.tci
    • dm6446_dvsdk_combos_2_03/packages/ti/sdo/servers/
      • decode/decode.tcf
      • encode/encode.tcf
      • loopback/loopback.tcf

    but after

    • make dsplink_clean demos_clean codecs_clean
    • make dsplink codecs demos
    • make install

    it still tells me configuration mismatch.

    I added armDspLinkConfig:

    • osalGlobal.armDspLinkConfig = {
    •     memTable: [
    •         ["DDRALGHEAP",   {addr: 0x88000000, size: 0x07A00000, type: "other"}],
    •         ["RESET_VECTOR", {addr: 0x8FF00000, size: 0x00000080, type: "reset"}],
    •         ["DDR2",         {addr: 0x8FA00000, size: 0x00400000, type: "main" }],
    •         ["DSPLINKMEM",   {addr: 0x8FE00000, size: 0x00100000, type: "link" }],
    •     ],
    • };

    under

    • var osalGlobal = xdc.useModule('ti.sdo.ce.osal.Global');

    in "dvsdk_demos_2_00_00_04/dm6446/decode/decode.cfg", but it didn't work either.

    How do I check the memory map configuration at run time? Is the output

    • @1,304,719us: [+2 T:0x40be0490 S:0x40bdfd44] OP - Processor_create_d> Adding DSP segment #0 to Link configuration: name='DDR2', startAddress=0x8fa00000, sizeInBytes=0x400000, shared=1, syncd=0
    • @1,304,932us: [+2 T:0x40be0490 S:0x40bdfd44] OP - Processor_create_d> Adding DSP segment #1 to Link configuration: name='DSPLINKMEM', startAddress=0x8fe00000, sizeInBytes=0x100000, shared=1, syncd=0
    • @1,305,140us: [+2 T:0x40be0490 S:0x40bdfd44] OP - Processor_create_d> Adding DSP segment #2 to Link configuration: name='RESET_VECTOR', startAddress=0x8ff00000, sizeInBytes=0x80, shared=1, syncd=0
    • @1,305,350us: [+2 T:0x40be0490 S:0x40bdfd44] OP - Processor_create_d> Adding DSP segment #3 to Link configuration: name='DDRALGHEAP', startAddress=0x88000000, sizeInBytes=0x7a00000, shared=0, syncd=0

    DSP side or ARM side? How do I check the other side at run time to see the configured memory map because dmesg only tells me to compare but doesn't tell me what to search for?

    tkx for answering!

  • Hi,

    RidgeRun SDK for DM6446 uses the LSP 2.00 kernel (2.6.18) or Git (2.6.30), which version is basically up to the customer requirements. We currently offer support for the 2.6.18 using the DVSDK 2.00 early releases and have costumers successfully using them to develop their products. The free version includes the integration of the DVSDK in the build system.

    Regards,

    Diego

     

  • Palatis,

    I finally got around to trying out dvsdk_2_0_0_18 on our DM6446 EVM and was successful in running the demos.  All I did was install the dvsdk per the Getting Started Guide (GSG) and configure my u-boot to load linux kernel via TFTP (optionally you can flash to NOR or NAND flash) and mount file system via NFS (again, other options here). 

    Then, I made sure I ran loadmodules.sh before running demos; did you do this step?  When I did this I got a minor error suggesting CMEM was overlapping Linux Kernel memory; therefore I reduced the size of the memory for the Linux kernel  to overcome this minor issue (FYI, change u-boot bootargs variable to include 'MEM=112M' instead of 'MEM=120M', although I believe 118M would have worked).  After making this minor change in u-boot's bootargs variable, I rebooted the EVM, ran loadmodules.sh, and ran the demos without any issues.

    To answer your question about where to define memory map, it is defined piece by piece in several places; for example the bootargs I just mentioned above defines the size of the Linux kernel in the overall memory map.  The following wiki article should give you a good understanding of how a system integrator may decide to define the memory map for the entire system and how he would go about configuring his memory map in the various software components involved: http://tiexpressdsp.com/index.php?title=Changing_the_DVEVM_memory_map

    However, please note per my comments above that the only thing I changed was the Linux Kernel memory space and was able to run the demos without any issues with the DVSDK software.

  • I'm using the demo target system dl-ed from

    • https://www-a.ti.com/downloads/sds_support/targetcontent/dvsdk/mv_dvsdk/v2_00/exports/restore_dm6446/mvltarget5_0_0801921_update.tar.gz

    and the pre-build binaries from

    • https://www-a.ti.com/downloads/sds_support/targetcontent/dvsdk/mv_dvsdk/v2_00/exports/restore_dm6446/overlay.tar.gz

    Steps taken:

    1. untar mvltarget5_0_0801921_update.tar.gz to /home/sysroot/mvl50_rootfs using the root user.
    2. untar overlay.tar.gz to /home/sysroot/mvl50_rootfs/opt, so i get /home/sysroot/mvl50_rootfs/opt/dvsdk/dm6446/* files.
    3. copy /home/sysroot/mvl50_rootfs/boot/uImage-ti-davinci_evm-arm_v5t_le-2.6.18_pro500-1.2.1.0801921 to my tftp dir so u-boot can find it and dl it.
    4. modify u-boot env so my board boots with the kernel and the rootfs...
      1. setenv bootfile uImage-ti-davinci_evm-arm_v5t_le-2.6.18_pro500-1.2.1.0801921
      2. setenv bootargs console=ttyS0,115200n8 noinitrd rw ip=192.168.1.113:192.168.1.254:192.168.1.1:255.255.255.0:DM6446-A03:eth0:off nfsroot=192.168.1.254:/home/sysroot/mvl50_rootfs,nolock root=/dev/nfs mem=112M
      3. dhcp
      4. bootm
    5. boots into MVL 5.0 pro...
    6. cd into /opt/dvsdk/dm6446 and run ./loadmodules.sh, dmesg output:
      1. ioremap_nocache(0x87600000, 10485760)=0xc8000000
      2. allocated heap buffer 0xc8000000 of size 0x2c000
      3. cmem initialized 5 pools between 0x87600000 and 0x88000000
      4. dsplinkk: no version for "struct_module" found: kernel tainted.
      5. DSPLINK Module (1.60) created on Date: Oct 24 2008 Time: 12:59:07
    7. run ./encode -s test.g711 and get a kernel panic like the above post mentioned.

    I'm not even building any binaries by myself but using only the provided pre-built binaries. which step did i go wrong?

    or am I just having bad luck?

  • Palatis,

    I did not try those files; I figure it would be safer to stick to the ones mentioned in the Getting Started Guide; for example 'mvl_5_0_0_demo_lsp_setuplinux_#_#_#_#' mentioned in the GSG already gives you your target file system; therefore there is no need to download or install 'mvltarget5_0_0801921_update.tar.gz'; I am not saying your approach should not work, but since the process on how to use 'mvltarget5_0_0801921_update.tar.gz ' is not documented in the GSG it requires some assumptions about this file which may not hold true; therefore I did not try this path.  I would recomend you stick to the GSG.

  • Ohh... Juan, no offence, but...

    Please believe me, I've already tried all possible combinations and all possible paths I could've thought of, but just can't never get them working. That's why I'm asking the question here.

    Of course I tried the method that's mentioned in GSG, too. It just didn't work out. And the method specified in GSG is far more complex and it's hard to describe it here in a few steps (else there won't be a whole "guide" to describe it.), that's why I just try to show you with a pre-built target-filesys and pre-built demo binaries.

    maybe I'm just having bad luck >___<

  • no offense taken, :)  we are here to help.  FYI, I have been installing software for DM6446 for over three years (since we launched this platform) and I know it can be complex.  However, please note I have personally confirmed the software works on my end so I am sure we can get to the bottom of the issue you are seeing.  Like I suggested, I tried to follow the GSG but I have done this so many times that I do not read the GSG in its entirety.  I will give the software in the files you mentioned above a try next week when I am back in the office, and see what I get; but from past experience, I would feel much more comfortable recommending the software mentioned in the getting started guide.  Thank you for your patience.

  • Emm... I've been using Linux primarily as desktop and server system for over 7 years, you may call me a "geek" or "junior random hacker," so let's get to the problem the geeky way :) BTW I've read the "How to Ask Questions the Smart Way" guide (http://catb.org/esr/faqs/smart-questions.html) and trying hard not to ask dumb questions here. If I still do, please tell me :P

    I've tried several combinations of, dvsdk, kernel, dsplinkk.ko/cmemk.ko, dspbios, and CE, but all I got is crash/hang or "mismatched configuration," none of them work anyway. So the past few days I just sticked with

    all other stuff not mentioned here are provided with dvsdk, they are

    • codec_engine_2_21
    • dm6446_dvsdk_combos_2_03
    • dvsdk_demos_2_00_00_04
    • linuxutils_2_22_01
    • dsplink-1_60-prebuilt

    But anyway no matter what versions they are, they all failed. Summary:

    1. First I tried the pre-built target system and pre-built binaries mentioned in previous posts, they produce kernel panics.
    2. Second I tried to build the kernel and kernel modules with the montavista 5.0 toolchain provided on the page you gave me, with  the target system and pre-built binaries, but they produce the same kernel panic.
    3. Third I tried to build the demo and codec binaries too, I did `make codecs_clean dsplink_clean demos_clean && make dsplink_dsp codecs demos && make install`, but they
      • produce the same kernel panic with production codecs
      • "mismatched configuration" if I `mv encodeCombo_e.x64P encodeCombo.x64P`
    4. Then I tried to build everything (kernel, module, userspace) with my own compiler (Gentoo armv5tel-softfloat-linux-gnueabi-gcc 4.3.3), but they kernel panic too.

    So basically no matter what I do, I get the *same* kernel panic, but this isn't mentioned in any of the documents (google returned no result either). That's why I'm wondering what I did wrong...

  • I do not have my DVSDK setup with me at the moment (can confirm on Monday), so I am relying on the release notes.  Based on this, the biggest thing that stands out is that the docs claim DVSDK 2.0.0.18 includes PSP_02_00_00_100 instead of LSP_02_00_00_110 you mentioned above; again, without having my setup I cannot verify this.  All other components you mention seem to match, althought I see some key components missing such as framework_components_2_21; I assume you have these and simply did not mention them.

     

     

  • ok, just to give you an update as promised.  I downloaded the following files from https://www-a.ti.com/downloads/sds_support/targetcontent/dvsdk/mv_dvsdk/v2_00/index_external.html

    04/13/2009  02:12 PM       128,413,511 bios_setuplinux_5_33_02.bin
    04/13/2009  01:56 PM       662,950,466 data.tar.gz
    04/13/2009  01:35 PM       301,836,892 dvsdk_setuplinux_2_00_00_18.bin
    04/13/2009  01:54 PM        27,795,993 linux_performance_testbench_setup_02.01.02.00.bin
    04/13/2009  01:39 PM     1,014,724,602 mvl_5_0_0801921_demo_sys_setuplinux.bin
    04/13/2009  01:54 PM        60,722,702 mvl_5_0_0_demo_lsp_setuplinux_02_00_00_110.bin
    04/13/2009  02:11 PM        28,552,697 TI-C6x-CGT-v6.0.21.1.bin
    04/13/2009  02:11 PM       126,262,764 xdctools_setuplinux_3_10_03.bin

    I installed these files per the Getting Started Guide (GSG) and after installation my Linux Host root DVSDK directory included the following

    bin

    bios_5_33_02

    biosutils_1_01_00

    ceutils_1_06

    cg6x_6_0_21

    cg_xml_2_12_00

    clips

    codec_engine_2_21

    dm355_2_00_00_18_release_notes.html

    dm355_codecs_1_13_000

    dm6446_2_00_00_18_release_notes.html

    dm6446_dvsdk_combos_2_03

    dm6467_2_00_00_18_release_notes.html

    dm6467_dvsdk_combos_2_03

    dmai_1_20_00_06

    docs

    dsplink-1_60-prebuilt

    dvsdk_demos_2_00_00_04

    dvtb_4_00_04

    edma3_lld_1_05_00

    examples

    framework_components_2_21

    kernel_binaries

    licenses

    linuxutils_2_22_01

    Makefile

    mapdmaq

    mapdmaq-hd

    PSP_02_00_00_110

    quilt

    Rules.make

    uninstall

    xdais_6_22_01

    xdctools_3_10_03

  • yes i'm having exactly the same files.

  • If this is the case, then there is likely a minor error during your installation process.  Another possibility could be a corrupted file system.. which can be fixed by copying files system over again (step 4 in section 4.3.5 of GSG) and doing make isntall on root dvsdk directory again (step 3, in section 4.6 of GSG).

    Do you get any errors when running loadmodules.sh (right before demos)?  If so, this could point to an iconpatibility between your kernel and filesystem.  But if you can get past loadmodules, then the issue is likely in your file-system.

  • yes i thought it was a nfs error, too, so I did

    • mkdir /mnt/demo
    • mount tmpfs /mnt/demo -t tmpfs

    and copy the demo files over, but then the kernel oops in the shmfs subsystem.

    and yes, I can lodamodule.sh without any problem, it's encode/decode which are not working.

  • I would recommend re-installing the file-system (mvl_5_0_0801921_demo_sys_setuplinux.bin and dvsdk_setuplinux_2_00_00_18.bin files) instead of just copying things over again; it is looking more and more like a filesystem issue and we do not know if the copy may be bad as well.