Tool/software: Linux
Support,
I want to run the AM5728 EVM camera demos and I'm having trouble getting it to work. I've downloaded the latest SDK image, 4.03, and created an sd-card through windows. When i goto OpenCL demo through MATRIX GUI, it seems to connect to the camera but then screen flashes white and goes back to default MATRIX screen?
I have seen a few posts recommending to apply a patch, one says "use PLSDK 4.04" when latest SDK is 4.03? I do not have the SDK installed on a linux host and therefore cannot apply any patches, or rebuild once a patch is applied.
I would like a link to a pre-built image that has the SDK/Camera fixes already applied.
Thanks.