This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 TI Spectrum Evaluation Board (EVM) Uart1 Pins



Hi, 

Can any one tell me whether the DM365 EVM board has accessable points to the Uart1 RX and TX lines?

I know the DM365 IC supports it over pins (V4,T1 or E4,E1), however, do these go to any jumper on the EVM onto which I can connect. I have looked in the Technical Reference Manual hoping to find them on jumper J10 (imager interface), however, I don't think GIO17 and GIO16 are the same as GPIO17 and GPIO16. Could some please explain the difference to me? 

Thanks, 

Manfred

Edit: Sorry, please move this post to the hardware section