I am trying learn how to recompile the UBL for DM355 so that I can start 'tweaking' it to fit my hardware configuration.
To import the project I copied the flash_utils folder to a temp folder on my computer and imported "UBL_NAND.pjt" project from "flash_utils\DM35x_Rev_C\CCS\UBL" folder.
I get two error messages during UBL 'Build All':
errors encountered during linking;
"C:/pub/pub/flash_utils/DM35x_Rev_C/CCS/UBL/NAND/UBL_DM355_NAND_216.out"
not built UBL_NAND line 0 1286828249859 76 unresolved symbol __TI_zero_init UBL_NAND line 0 1286828249859 74 |
The Console window has the following output:
<Linking> warning: creating output section ".cinit" without a SECTIONS specification undefined first referenced symbol in file --------- ---------------- __TI_zero_init error: unresolved symbols remain warning: entry-point symbol other than "_c_int00" specified: "boot" error: errors encountered during linking; "C:/pub/pub/flash_utils/DM35x_Rev_C/CCS/UBL/NAND/UBL_DM355_NAND_216.out" not built >> Compilation failure C:\Program Files\Texas Instruments\ccsv4\utils\gmake\gmake: *** [C:/pub/pub/flash_utils/DM35x_Rev_C/CCS/UBL/NAND/UBL_DM355_NAND_216.out] Error 1 C:\Program Files\Texas Instruments\ccsv4\utils\gmake\gmake: Target `all' not remade because of errors. Build complete for project UBL_NAND |
What am I doing wrong?