Part Number: TMS320C6455
Other Parts Discussed in Thread: STRIKE
Hi,
I'm trying to create some P.O.S.T. code for an 6455 design, and I'd like to be able to check that the DSP is receiving a sensible 25 MHz clock on CLKIN2. The application here is fairly minimal, for instance, no DSP/BIOS available.
I believe that CLKIN2 feeds PLL2 and generates SYSREFCLK, SYSCLK1, and the DDR Clock. Ideally I'd like to be able to read a counter register that is incremented by something derived from CLKIN2 at two distinct points in my code and check that the register has incremented by the appropriate amount in between, but I can't find anything like that I could use. A refresh count-down on the DDR controller would do, but I can't find such a register.
Anyone got any suggestions?
B.R.
Paul