Hi, all
on evm2 board, when suspend/wakeup frequently, the usb host could not function.
and sometimes output the below function:
!!!CFunction( tier 1)::IsPipeHalted on suspend state is illgle, address = 1, pipe = 0.
Any suggestion ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, all
on evm2 board, when suspend/wakeup frequently, the usb host could not function.
and sometimes output the below function:
!!!CFunction( tier 1)::IsPipeHalted on suspend state is illgle, address = 1, pipe = 0.
Any suggestion ?
Huai,
There is a known issue with the EHCI port on the 6.15 release and the symptoms of that issue match those mentioned in your post.
Bug ID is 74790.
Details of TI bug database are as below (this link is present in the release notes). You can track the status of the bug at:
Note: If prompted for login/password, please close the browser and click on the link again.
Having said that, could you provide details about your setup? Your responses would help in knowing whether this is the same issue that is documented in the bug.
Hi,
I could not access the website you said, clicking the site serveral times.
Below is my details:
1, I use otg and host ports both
2, for otg, it is a slave , connecting for PC. and , for host, it is master, and connect a card reader.
3, generally speaking, pressed the pwr_on button about twenty times, it will occurs. and very freqently
The link should work fine. You can clear your browser cache, close the browser and try again. Alternately if you are stuck at the login screen then try this.
Login: readonly
Password: readonly
Schema Repository: SDO-WEB
Database: SDOWP
This will lead you to a very generic page. Select Public Queries -> Embedded Software -> WinCE -> BSP_WINCE_OMAP35X_Active_IRs
Regarding #2. Does the behavior change if you only have OTG or EHCI host connected (i.e, don't connect to both OTG and EHCI ports). This will give us another data point.
Thanks.