This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDK 1.92, network examples

hello all,

if anyone worked on NDK 1.92 networking examples then plz tell me in ALE_NORMAL mode, packets from both ports are rcv'd and xmt'd. but when i have converted its mode from normal to bypass it stops packet transmission.

when i call the function llpacketsend in DequeueRx(), it receives pakets from only port 0 and send it to both ports. it stops receiving packet from port 1. what should be its reason?

also can anyone tell me which field in handles shows that packet has been received and which field in handles shows that packet has been transmitted?

plz help me.

regards

adnan