This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5716: DSP memory initialization

Part Number: AM5716


Tool/software: Linux

Hello,

I am using TI gel script to init both of ARM and DSP core on AM5716. DSP uses TI rtos, and ARM core uses linux.  The script I used are: AM571x_dsp_startup.gel  I see it basically just do a memory init. and it works fine when I download my dsp build using emulator.

In our real application, the DSP build will be loaded by linux core in ARM core. To my understand, the memory init should be done before DSP build is loaded to DSP core? if so,  memory init job as following code in script: has to be done by linux kernel before it load DSP up?

/*******************************************************************/
/* This GEL file is loaded on the command line of Code Composer */
/* The StartUp() function is called every time you start */
/* Code Composer. You can customize this function to */
/* initialize wait states or to perform other initialization. */
/* */
/* AM571x C66x DSP */
/* */
/* */
/*******************************************************************/


#define WR_MEM_32(addr, data) *(unsigned int*)(addr) =(unsigned int)(data)
#define RD_MEM_32(addr) *(unsigned int*)(addr)
#define uint32_t unsigned int

StartUp()
{
GEL_TextOut("--->>> AM571x C66x DSP Startup Sequence In Progress... <<<---\n");

/*------------------ Memory Map Config -------------------*/
GEL_MapOff();
GEL_MapReset();
memorymap_init();
GEL_MapOn();

/*------------------ Load Common Gel Files -------------------*/
GEL_LoadGel("$(GEL_file_dir)//AM571x_dsp_basic_emulation.gel");

GEL_TextOut("--->>> AM571x C66x DSP Startup Sequence DONE! <<<---\n");
}

memorymap_init()
{
GEL_MapAddStr(0x00800000, 0, 0x00800000, "R|W|AS4", 0); /* DSP RAM Access 288K (L2 RAM) + 32K (L1P SRAM) + 32K (L1D SRAM)*/
GEL_MapAddStr(0x01BC0000, 0, 0x00001000, "R|W|AS4", 0); /* DSP EDM register - 4KBytes */
GEL_MapAddStr(0x01C20000, 0, 0x00001000, "R|W|AS4", 0); /* SYSC- CONFIG - 4KBytes */
GEL_MapAddStr(0x01C21000, 0, 0x00001000, "R|W|AS4", 0); /* WUGEN - 4KBytes */
GEL_MapAddStr(0x01C30000, 0, 0x00000100, "R|W|AS4", 0); /* L1 config register - 256Bytes */
GEL_MapAddStr(0x01C30200, 0, 0x00000100, "R|W|AS4", 0); /* L2 config register - 256Bytes */
GEL_MapAddStr(0x01C30400, 0, 0x00000200, "R|W|AS4", 0); /* Unicache debug - 512Bytes */
GEL_MapAddStr(0x01C30800, 0, 0x00000800, "R|W|AS4", 0); /* Attr MMU - 2KBytes */
GEL_MapAddStr(0x01D10000, 0, 0x00010000, "R|W|AS4", 0); /* 3PCC CONFIG - 64KBytes */
GEL_MapAddStr(0x01D05000, 0, 0x00000400, "R|W|AS4", 0); /* 3PTC0- CONFIG - 1KBytes */
GEL_MapAddStr(0x01D06000, 0, 0x00000400, "R|W|AS4", 0); /* 3PTC1- CONFIG - 1KBytes */
GEL_MapAddStr(0x01800000, 0, 0x00010000, "R|W|AS4", 0); /* Interrupt controller - 64KBytes */
GEL_MapAddStr(0x01810000, 0, 0x00001000, "R|W|AS4", 0); /* DSP Securty ID - 4KBytes */
GEL_MapAddStr(0x01812000, 0, 0x00001000, "R|W|AS4", 0); /* DSP Revision ID - 4KBytes */
GEL_MapAddStr(0x01840000, 0, 0x00010000, "R|W|AS4", 0); /* DSP Cache CFG and MAR registers */
GEL_MapAddStr(0x01D00000, 0, 0x00020000, "R|W|AS4", 0); /* ABE NC L4 S3220 */
GEL_MapAddStr(0x01D28000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC McASP1 CFG Port */
GEL_MapAddStr(0x01D29000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC McASP1 CFG - L4 interconnect */
GEL_MapAddStr(0x01D2A000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC McASP1 DATA Port */
GEL_MapAddStr(0x01D2B000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC McASP1 DATA - L4 interconnect */
GEL_MapAddStr(0x01D2C000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC SLIMBUS1 - module */
GEL_MapAddStr(0x01D2D000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC SLIMBUS1 - L4 interconnect */
GEL_MapAddStr(0x01D2E000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC DMIC - module */
GEL_MapAddStr(0x01D2F000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC DMIC - L4 interconnect */
GEL_MapAddStr(0x01D30000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC WDT3 - module */
GEL_MapAddStr(0x01D31000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC WDT3 - L4 interconnect */
GEL_MapAddStr(0x01D32000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC McPDM - module */
GEL_MapAddStr(0x01D33000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC McPDM - L4 interconnect */
GEL_MapAddStr(0x01D38000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC GPTIMER5 - module */
GEL_MapAddStr(0x01D39000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC GPTIMER5 - L4 interconnect */
GEL_MapAddStr(0x01D3A000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC GPTIMER6 - module */
GEL_MapAddStr(0x01D3B000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC GPTIMER6 - L4 interconnect */
GEL_MapAddStr(0x01D3C000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC GPTIMER7 - module */
GEL_MapAddStr(0x01D3D000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC GPTIMER7 - L4 interconnect */
GEL_MapAddStr(0x01D3E000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC GPTIMER8 - module */
GEL_MapAddStr(0x01D3F000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC GPTIMER8 - L4 interconnect */
GEL_MapAddStr(0x01D80000, 0, 0x00010000, "R|W|AS4", 0); /* ABE NC DMEM - module */
GEL_MapAddStr(0x01D90000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC DMEM - L4 interconnect */
GEL_MapAddStr(0x01DA0000, 0, 0x00010000, "R|W|AS4", 0); /* ABE NC CMEM - module */
GEL_MapAddStr(0x01DB0000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC CMEM - L4 interconnect */
GEL_MapAddStr(0x01DC0000, 0, 0x00010000, "R|W|AS4", 0); /* ABE NC SMEM - module */
GEL_MapAddStr(0x01DD0000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC SMEM - L4 interconnect */
GEL_MapAddStr(0x01DE0000, 0, 0x00010000, "R|W|AS4", 0); /* ABE NC PMEM - module */
GEL_MapAddStr(0x01DF0000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC PMEM - L4 interconnect */
GEL_MapAddStr(0x01DF1000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC AESS - module */
GEL_MapAddStr(0x01DF2000, 0, 0x00001000, "R|W|AS4", 0); /* ABE NC AESS - L4 interconnect */
GEL_MapAddStr(0x01E00000, 0, 0x00100000, "R|W|AS4", 0); /* IVA-HD - 1MBytes */
GEL_MapAddStr(0x01F00000, 0, 0x00100000, "R|W|AS4", 0); /* OCP Interconnect Registers - 1MBytes */
GEL_MapAddStr(0x10800000, 0, 0x00020000, "R|W|AS4", 0); /* SL2->L1 - 128KBytes */
GEL_MapAddStr(0x10820000, 0, 0x00020000, "R|W|AS4", 0); /* SL2->L2 - 128KBytes */
GEL_MapAddStr(0x10900000, 0, 0x00040000, "R|W|AS4", 0); /* SL2 locked Region - 256KBytes */

GEL_MapAddStr(0x10D00000, 0, 0x00004000, "R|W|AS4", 0); /* ABE L4 S3220 */
GEL_MapAddStr(0x10D22000, 0, 0x00001000, "R|W|AS4", 0); /* ABE McBSPLP1 - module */
GEL_MapAddStr(0x10D23000, 0, 0x00001000, "R|W|AS4", 0); /* ABE McBSPLP1 - L4 interconnect */
GEL_MapAddStr(0x10D24000, 0, 0x00001000, "R|W|AS4", 0); /* ABE McBSPLP2 - module */
GEL_MapAddStr(0x10D25000, 0, 0x00001000, "R|W|AS4", 0); /* ABE McBSPLP2 - L4 interconnect */
GEL_MapAddStr(0x10D26000, 0, 0x00001000, "R|W|AS4", 0); /* ABE McBSPLP3 - module */
GEL_MapAddStr(0x10D27000, 0, 0x00001000, "R|W|AS4", 0); /* ABE McBSPLP3 - L4 interconnect */
GEL_MapAddStr(0x10D28000, 0, 0x00001000, "R|W|AS4", 0); /* ABE McASP1 CFG Port */
GEL_MapAddStr(0x10D29000, 0, 0x00001000, "R|W|AS4", 0); /* ABE McASP1 CFG - L4 interconnect */
GEL_MapAddStr(0x10D2A000, 0, 0x00001000, "R|W|AS4", 0); /* ABE McASP1 DATA Port */
GEL_MapAddStr(0x10D2B000, 0, 0x00001000, "R|W|AS4", 0); /* ABE McASP1 DATA - L4 interconnect */
GEL_MapAddStr(0x10D2C000, 0, 0x00001000, "R|W|AS4", 0); /* ABE SLIMBUS1 - module */
GEL_MapAddStr(0x10D2D000, 0, 0x00001000, "R|W|AS4", 0); /* ABE SLIMBUS1 - L4 interconnect */
GEL_MapAddStr(0x10D2E000, 0, 0x00001000, "R|W|AS4", 0); /* ABE DMIC - module */
GEL_MapAddStr(0x10D2F000, 0, 0x00001000, "R|W|AS4", 0); /* ABE DMIC - L4 interconnect */
GEL_MapAddStr(0x10D30000, 0, 0x00001000, "R|W|AS4", 0); /* ABE WDT3 - module */
GEL_MapAddStr(0x10D31000, 0, 0x00001000, "R|W|AS4", 0); /* ABE WDT3 - L4 interconnect */
GEL_MapAddStr(0x10D32000, 0, 0x00001000, "R|W|AS4", 0); /* ABE McPDM - module */
GEL_MapAddStr(0x10D33000, 0, 0x00001000, "R|W|AS4", 0); /* ABE McPDM - L4 interconnect */
GEL_MapAddStr(0x10D38000, 0, 0x00001000, "R|W|AS4", 0); /* ABE GPTIMER5 - module */
GEL_MapAddStr(0x10D39000, 0, 0x00001000, "R|W|AS4", 0); /* ABE GPTIMER5 - L4 interconnect */
GEL_MapAddStr(0x10D3A000, 0, 0x00001000, "R|W|AS4", 0); /* ABE GPTIMER6 - module */
GEL_MapAddStr(0x10D3B000, 0, 0x00001000, "R|W|AS4", 0); /* ABE GPTIMER6 - L4 interconnect */
GEL_MapAddStr(0x10D3C000, 0, 0x00001000, "R|W|AS4", 0); /* ABE GPTIMER7 - module */
GEL_MapAddStr(0x10D3D000, 0, 0x00001000, "R|W|AS4", 0); /* ABE GPTIMER7 - L4 interconnect */
GEL_MapAddStr(0x10D3E000, 0, 0x00001000, "R|W|AS4", 0); /* ABE GPTIMER8 - module */
GEL_MapAddStr(0x10D3F000, 0, 0x00001000, "R|W|AS4", 0); /* ABE GPTIMER8 - L4 interconnect */
GEL_MapAddStr(0x10D80000, 0, 0x00010000, "R|W|AS4", 0); /* ABE DMEM - module */
GEL_MapAddStr(0x10D90000, 0, 0x00001000, "R|W|AS4", 0); /* ABE DMEM - L4 interconnect */
GEL_MapAddStr(0x10DA0000, 0, 0x00010000, "R|W|AS4", 0); /* ABE CMEM - module */
GEL_MapAddStr(0x10DB0000, 0, 0x00001000, "R|W|AS4", 0); /* ABE CMEM - L4 interconnect */
GEL_MapAddStr(0x10DC0000, 0, 0x00010000, "R|W|AS4", 0); /* ABE SMEM - module */
GEL_MapAddStr(0x10DD0000, 0, 0x00001000, "R|W|AS4", 0); /* ABE SMEM - L4 interconnect */
GEL_MapAddStr(0x10DE0000, 0, 0x00010000, "R|W|AS4", 0); /* ABE PMEM - module */
GEL_MapAddStr(0x10DF0000, 0, 0x00001000, "R|W|AS4", 0); /* ABE PMEM - L4 interconnect */
GEL_MapAddStr(0x10DF1000, 0, 0x00001000, "R|W|AS4", 0); /* ABE AESS - module */
GEL_MapAddStr(0x10DF2000, 0, 0x00001000, "R|W|AS4", 0); /* ABE AESS - L4 interconnect */

GEL_MapAddStr(0x10E00000, 0, 0x00004000, "R|W|AS4", 0); /* ABE Locked Region L4 S3220 */
GEL_MapAddStr(0x10E22000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region McBSPLP1 - module */
GEL_MapAddStr(0x10E23000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region McBSPLP1 - L4 interconnect */
GEL_MapAddStr(0x10E24000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region McBSPLP2 - module */
GEL_MapAddStr(0x10E25000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region McBSPLP2 - L4 interconnect */
GEL_MapAddStr(0x10E26000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region McBSPLP3 - module */
GEL_MapAddStr(0x10E27000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region McBSPLP3 - L4 interconnect */
GEL_MapAddStr(0x10E28000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region McASP1 CFG Port */
GEL_MapAddStr(0x10E29000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region McASP1 CFG - L4 interconnect */
GEL_MapAddStr(0x10E2A000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region McASP1 DATA Port */
GEL_MapAddStr(0x10E2B000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region McASP1 DATA - L4 interconnect */
GEL_MapAddStr(0x10E2C000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region SLIMBUS1 - module */
GEL_MapAddStr(0x10E2D000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region SLIMBUS1 - L4 interconnect */
GEL_MapAddStr(0x10E2E000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region DMIC - module */
GEL_MapAddStr(0x10E2F000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region DMIC - L4 interconnect */
GEL_MapAddStr(0x10E30000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region WDT3 - module */
GEL_MapAddStr(0x10E31000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region WDT3 - L4 interconnect */
GEL_MapAddStr(0x10E32000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region McPDM - module */
GEL_MapAddStr(0x10E33000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region McPDM - L4 interconnect */
GEL_MapAddStr(0x10E38000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region GPTIMER5 - module */
GEL_MapAddStr(0x10E39000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region GPTIMER5 - L4 interconnect */
GEL_MapAddStr(0x10E3A000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region GPTIMER6 - module */
GEL_MapAddStr(0x10E3B000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region GPTIMER6 - L4 interconnect */
GEL_MapAddStr(0x10E3C000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region GPTIMER7 - module */
GEL_MapAddStr(0x10E3D000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region GPTIMER7 - L4 interconnect */
GEL_MapAddStr(0x10E3E000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region GPTIMER8 - module */
GEL_MapAddStr(0x10E3F000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region GPTIMER8 - L4 interconnect */
GEL_MapAddStr(0x10E80000, 0, 0x00010000, "R|W|AS4", 0); /* ABE Locked Region DMEM - module */
GEL_MapAddStr(0x10E90000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region DMEM - L4 interconnect */
GEL_MapAddStr(0x10EA0000, 0, 0x00010000, "R|W|AS4", 0); /* ABE Locked Region CMEM - module */
GEL_MapAddStr(0x10EB0000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region CMEM - L4 interconnect */
GEL_MapAddStr(0x10EC0000, 0, 0x00010000, "R|W|AS4", 0); /* ABE Locked Region SMEM - module */
GEL_MapAddStr(0x10ED0000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region SMEM - L4 interconnect */
GEL_MapAddStr(0x10EE0000, 0, 0x00010000, "R|W|AS4", 0); /* ABE Locked Region PMEM - module */
GEL_MapAddStr(0x10EF0000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region PMEM - L4 interconnect */
GEL_MapAddStr(0x10EF1000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region AESS - module */
GEL_MapAddStr(0x10EF2000, 0, 0x00001000, "R|W|AS4", 0); /* ABE Locked Region AESS - L4 interconnect */

GEL_MapAddStr(0x20000000, 0, 0xE0000000, "R|W|AS4", 0); /* External - SOC Mems andPeripherals - 3.5GBytes */

GEL_MapAddStr(0x80000000, 0, 0x40000000, "R|W|AS4", 0); /* External - EMIF1 - 1GBytes */
}

OnReset()
{

}

OnResetDetected()
{

GEL_TextOut( "Core Reset has occurred.\n\n" );
}

OnTargetConnect()
{

}

Thanks in advance!

Ron