Hi ,
I followed the steps given in the above mentioned link i.e
processors.wiki.ti.com/.../Linux_IPC_on_AM57xx
I added IPC to my existing DSP SYS/BIOS project, I could generate a binary file with extension being '".out", in the above provided wiki page it is mentioned that ".xe66" format binary is to be linked and added in firmware folder of the linux master (ARM A15 core).
So, is both ".out" and ".xe66" extensions same?
Also, is it possible to dump binaries to to DSP core of Sitara AM57XX core through JTAG?
Can anyone please elaborate how to make the master core (ARM A15) running on linux to dump binaries to the slave core (DSP) using the binaries generated from the "IPC added DSP SYS/BIOS" project (binaries generated using CCS).
Thanks and Regards,
Janardan M