Hello,
I was reading Chli post on DEEP SLEEP power consumption.
OMAP-L138 Power Consumption in DEEPSLEEP
1/Do you have any idea of typical power consumption of one PRU unit running?
(something like deep sleep mode but with one PRU running to monitor external event and wake the DSP only)
I was thinking using one PRU to wake up the DSP on my system but I can't find any info on power hungryness of the solution.
2/Do you have any idea of waking up time for DSP when receiving event from PRU
And waking up time from deep sleep?
3/ In deep sleep mode, I think mDDR content is preserved?
If i well understood you can even select how much ram you want to preserve, right?
If yes, does it means that in deep sleep mode, system consume around 30mW but the Linux system can be waken up is less than < xxx ms?
Thanks for any feedback on these subjects.
Regards,
Laurent