This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need confirmation of which SPI signals are used for SPI boot mode on C6748

I would like to get confirmation of which signals are required for support of the SPI boot modes on the C6748.  My specific situation is to use SPI1, but I would like confirmation for both SPI0 and SPI1.  The Using the TMS320C6748/C6746/C6742 Bootloader (Rev. C) guide does not specifically address the use of SPIx_ENA.

I would also suggest an update to the datasheet to indicate this information.

Please confirm the below.

Signal             Required?
SPI0_CLK           yes
SPI0_SIMO         yes
SPI0_SOMI         yes
SPI0_SCS[0]      yes
SPI0_ENA           no

SPI1_CLK           yes
SPI1_SIMO         yes
SPI1_SOMI         yes
SPI1_SCS[0]      yes
SPI1_ENA           no

Thank you.