Part Number: EVMK2H
Currently I am using EVMk2H board with mistral RTM BOC. I tested an internal loop back it successfully work. my question is "how to do external loopback ?"
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EVMK2H
Currently I am using EVMk2H board with mistral RTM BOC. I tested an internal loop back it successfully work. my question is "how to do external loopback ?"
hi,
I need to establish a AIF2 LTE CPRI on TCI6636k2H with mistral RTM BOC over optical cables. The problem arises in the project is "External loop back test " with optical cables.
1) what is the difference between internal loop back test and external loop back test?
2) Is there any changes need to do in the aif2 lte cpri example project code to implement a External loop back test?
The below console tells that result of the aif2 lte cpri example project code.
[C66xx_0] Beginning AIF2 LTE testing:
test: CPRI_4X_LTE_10MHZ
AIF CPRI mode
link 0 is disabled
link 1 is disabled
link 2 is disabled
link 3 runs at 4x rate
outbound data type: DL
outbound data width: 15 bit
inbound data type: DL
inbound data width: 15 bit
link 4 is disabled
link 5 is disabled
Number of monolithic packets received in RX queue channel0: 28
Number of monolithic packets in TX free queue for channel0: 28
Number of monolithic packets received in RX queue channel1: 28
Number of monolithic packets in TX free queue for channel1: 28
Test a) Monolithic Packet Data Recv: on chan: 0 are :28
Test a) Monolithic Packet Data Recv: on chan: 1 are :28
Test a) Monolithic Packet Data Send/Recv: PASS on channel: 2
Test b1) Monolithic Packet Tx Descriptor Counts:0 PASS
Test b2) Monolithic Packet Tx Complete Descriptor Counts:56 PASS
Test b3) Monolithic Packet Rx Descriptor Counts:0 PASS
Test b4) Monolithic Packet Rx Free Descriptor Counts:56 PASS
Ending CPRI_4X_LTE_10MHZ test
All tests have passed.
MCSDK 3.x for Keystone II devices(K2H, K2K, K2L, K2G & K2E)
CCSv5.5 is used