Hi,
I have bought OMAP based kit from TechNexion called the Tsunami.
I have installed the Win CE 6.0 R3 and all the updated. I have followed all the installation rules.
The developemnt system is Vista Home Premium Intel core 2 duo 2.0GHz with 4GB Ram and 64GB free HDD space.
I have added Microsoft USB web camera driver. On Building the system the process takes 9 hrs and seems to have stuck at one of the modules.
the build window has the following last lines.
NETCFV2_MODULES=dotnetv2 MEDIAAPPS_MODULES= wmpocx wmpocx_loc wmpocx_skin LN 811 I have to cancel the build on as the previous tries it has gone for 11 hours. Please guide thanks Regards Prasanna Mayekar