This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4376: DDR3 schematic questions

Part Number: AM4376

Hi SIr 

we used AM4376 for development an there are some questions as below 

1. The AM437x GP EVM has a 1K pull up to VDDS_DDR on the DDR_RESETn signal but the AM437x IDK/Starterkit does NOT have. 

    Which one is the correct setting? what condition to add 1K pull up  ?

2.After testing, we found that we need DDR_CKE to add pull up resistor to VDDR_VTT, Otherwise, it will cause system hang. what is the risk if we add pull up resistor?

    PS: IDK: DDR_CKE add 47 pull-up resistor to VDDR_VTT and  GP-EVM: DDR_CKE remove  47 pull-up resistor  to VDDR_VTT

BR

Yimin