This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H14: 10G PHY Selection

Part Number: 66AK2H14
Other Parts Discussed in Thread: TLK10034,

Hello, I am trying to find a PHY for the 10GIGE ports on the 66AK2H14 device and have found a TI part TLK10034. I know the ARM+DSP interface with XFI and the datasheet for the TLK10034 only states, "The device can also be used for optical physical layers (like 10GBASE-SR or 10GBASE-LR) by interfacing to optical modules requiring SFI or XFI electrical signaling." on page 156. Can anyone comment if this will be okay?

Thanks,

Joe

  • Hi Joe,

    If you're asking if you can use the TLK10034 device with the 66AK2H14 SoC, then yes it should be possible, see www.ti.com/.../spruho3a.pdf , Section 1.2 Industry Standards Compatibility:

    •Ten Gigabit Ethernet (10GbE): Supports the following electrical interfaces:
    – Supports XFI SFF INF-8077i spec (no SFP/SFP+)for 10Gb
    – Supports Serial-GMII (SGMII) Specification for 10/100/1000Mb
    – Supports 10GBase-KR Specification for 10Gb

    As for the statement in TLK10034, it says: Interface to Backplanes, Passive and Active Copper Cables, or SFP+ Optical Modules.

    Best Regards,
    Yordan