Other Parts Discussed in Thread: OMAP-L138, OMAP-L137, TPS65070
I noticed that the DaVinci-PSP-SDK-03.20.00.11 release for the OMAP-L138 uses the GPIO bit bang I2C driver instead of the hardware I2C driver. The board file for the OMAP-L137, however, uses the hardware I2C driver. Also, the Linux davinci git kernel has the OMAP-L138 using the hardware I2C driver. Is there a reason why the PSP release is using the big bang I2C driver? Is there a problem with the hardware or the hardware driver for the OMAP-L138?
Thanks,
Clif