Other Parts Discussed in Thread: THS8200, TIGER
Where and how is errata communicated to the customers?
Specifically, where are all the THS8200 errata documents located?
I was blindsided by a problem with the THS8200 vsync, now I see a post on this forum that the THS8200 will not meet timings at 1.8V ?? Where is this defect and workaround documented? I looked in the THS8200 product folder and there has been no released errata on the THS8200 since its introduction in 2002??
Yes, I see that the datasheet release has changed and with help of a post on this forum I see a subtle, cryptic caveat on page 90 of the datasheet that the syncs will not work at 3.3V. (how was I supposed to know to look here!?) Changing the datasheet without issuing an errata and informing customers is NOT satisfactory. Customers should proactively be notified of such things. Monitoring forums is not a very productive mechanism (for the customer).
---
Specifically related to this THS8200 problem...
- What is the problem?
- Where is the problem documented and its solution or workaround documented??
- Is the TI solution not to use the THS8200 with the DM6446?
- To use a level converter? (what about the phase delay?)
- Are there other signals (such as the clock) that have to be 3.3V?
- Can the DM6446's vs and hs be used?
- Same problem with the OMAP3?
- Was the THS8200 characterized at 1.8V? or are the datasheet specs just emperically derived on a lab bench?
- The DM6446 was released several years ago and the THS8200 even earlier. Is this the first that this has been noticed?