Part Number: AMIC120
Is AMIC120 able to run EtherCAT slave and Ethernet Tracer (TIDEP0064) simultaneously?
Regards, Bernd
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
You can't have the two features EtherCAT and Ethernet tracer run simultaneously on AMIC120.
The Ethernet traces is based on the Auto-forward with PRU Snoop function on PRU-ICSS1, see section 30.4.6.2.1.1 Auto-forward with Optional PRU Snoop on TRM.
The EtheCAT firmware is working on the forward port as on-the-fly, which is different form L2. EtherCAT firmware operates on byte or word base and is actively processing (receiving and transmitting byte by byte) the frame
If your question is to use ICSS_1 and ICSS_0 to have the two features, answer is negative as well as we don’t have RX_L2 buffer for MII ports from ICSS_0 available.
Regards,
Garrett
Garrett,
indeed I thought that with two ICSS it could be possible to run the two applications in parallel but you explained now why it isn't possible.
Thank you for the detailed answer.
Regards, Bernd