Hi:
I traine a SSD model changed on "github.com/tidsp/caffe-jacinto-models/tree/caffe-0.16/trained/object_detection/voc0712".
With quantStatusTool,the result is good,almost every target object is detected,But when I run the model on TDA2EXEVM,some object could't be detected in some frames.for example,as below
this result is runned with quantStatusTool;but the "1" object couldn't be detected with TIDL_OD usecase when runned on TDA2EXEVM.
And with quantStatusTool,I found the "1" object's confidence is 0.316087,so I set the "scoreThreshold" to 0.3 in TIDL_OD usecase,but the "1" object still couldn't be detected.
Is there something I missed?
My import config file is below:
# Default - 0
randParams = 0
# 0: Caffe, 1: TensorFlow, Default - 0
modelType = 0
# 0: Fixed quantization By tarininng Framework, 1: Dyanamic quantization by TIDL, Default - 1
quantizationStyle = 1
# quantRoundAdd/100 will be added while rounding to integer, Default - 50
quantRoundAdd = 25
numParamBits = 8
# 0 : 8bit Unsigned, 1 : 8bit Signed Default - 1
inElementType = 0
inputNetFile = "..\..\test\testvecs\config\caffe_modesl\ssd480x192\sparse\deploy.prototxt
inputParamsFile = "..\..\test\testvecs\config\caffe_modesl\ssd480x192\sparse\ssd480x192_sparse_iter_100000.caffemodel"
outputNetFile = "..\..\test\testvecs\config\tidl_models\tidl_net_jdetNet_480x192_ssd.bin"
outputParamsFile = "..\..\test\testvecs\config\tidl_models\tidl_param_jdetNet_480x192_ssd.bin"
rawSampleInData = 1
preProcType = 4
sampleInData = "..\..\test\testvecs\input\trace_480x192.y"
tidlStatsTool = "..\quantStatsTool\eve_test_dl_algo.out.exe"
layersGroupId = 0 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 2 1 2 1 2 1 2 1 2 1 2 1 2 1 2 1 2 1 2 2 2 2 2 2 2 0
conv2dKernelType = 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1
#conv2dKernelType = 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1
Regards