Part Number: AM5728
Hello,
I wanted to follow up on this previous support thread: https://e2e.ti.com/support/arm/sitara_arm/f/791/t/637820#pi316653=1
It was resolved with the following comment:
"These captures confirm that the issue is a DC-bias / DC ground reference problem on the driver side of the caps. This needs to be resolved with the manufacturer of the clock driver. I expect that some type of ground reference is needed due to a DC imbalance that saturates the driver."
However, earlier in the thread it was noted that this same distortion was measured on the TI RDK as well (using an LVDS clock driver). It was described as: "a scope-induced artifact. The delayed distortion is caused by the caps discharging very slowly thru the scope itself."
Using the same AM5728 module mentioned in the previous thread with another baseboard of ours, we were able to measure the same distortion of the clock when using a PI6C557-03 clock generator instead. This provides an HCSL output, which is properly terminated via 33 ohm series termination and 49.9 ohm termination resistors to ground to produce the DC bias.
At first it did seem like the probe load was affecting the clock termination/impedance. But I noticed that if you let the system boot up without the probe attached and wait for a short time, that the distortion will be immediately apparent as soon as the probe is connected to the test points. This seems to contradict the scope-induced artifact explanation, as the distortion seems to have occurred on its own rather than due to slowly discharging capacitors.
So we have three different clock generators, two of which meet LVDS or HCSL spec as described in the AM57x datasheet, and they all seem to become distorted after some time. Our measurements look pretty much the same as those given by the customer in the previously mentioned thread.
I was hoping that you might be able to comment further and help explain what the reason for this is. Any information would be much appreciated
Regards,
John Feuerstein