Other Parts Discussed in Thread: CCSTUDIO
Hello,
I had problems in compiler and the window showed me the following problems.
problem said:Warning: The project has no cmd file while the Text Linker is selected
[Linking...] "E:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -@"Debug.lkf"
<Linking>
>> warning: creating output section .gblinit without SECTIONS specification
>> warning: creating output section .mem without SECTIONS specification
>> warning: creating output section .rtdx_data without SECTIONS specification
>> warning: creating output section .sys without SECTIONS specification
>> warning: creating output section .clk without SECTIONS specification
>> warning: creating output section .hst1 without SECTIONS specification
>> warning: creating output section .hst without SECTIONS specification
>> warning: creating output section .pip without SECTIONS specification
>> warning: creating output section .hst0 without SECTIONS specification
>> warning: creating output section .hwi_vec without SECTIONS specification
>> warning: creating output section .swi without SECTIONS specification
>> warning: creating output section .printf without SECTIONS specification
>> warning: creating output section .sts without SECTIONS specification
>> warning: creating output section .tsk without SECTIONS specification
>> warning: creating output section .TSK_idle$stk without SECTIONS specification
>> warning: creating output section .idlcal without SECTIONS specification
>> warning: creating output section .idl without SECTIONS specification
>> warning: creating output section .LOG_system$buf without SECTIONS
specification
>> warning: creating output section .log without SECTIONS specification
>> warning: creating output section .sysinit without SECTIONS specification
>> warning: creating output section .vers without SECTIONS specification
>> warning: entry point symbol _c_int00 undefined
undefined first referenced
symbol in file
--------- ----------------
SWI_D_rdytab E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
IRAM$B E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_EXC_init E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_GBL_procId E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
__HOOK_knlId E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_KNL_exit E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
IRAM$L E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
TSK_VCREATEFXN E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_UTL_doError E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
PIP_F_start E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
GBL_boot E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
TSK_VDELETEFXN E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
KNL_glue E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_UTL_doAbort E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_HSRTDX_xmt E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
IDL_F_loop E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_CLK_DFLTMICROSECS E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_GBL_cacheInit64P E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_EXC_dispatch E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_CLK_htimePerLtime E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
GBL_stackbeg E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_CLK_D_tddr E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_UTL_doPutc E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_MEM E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
PRD_F_tick E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
__HOOK_NUMHOOKS E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_CLK_D_microseconds E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
RTA_F_or E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
TRC_R_mask E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
GBL_stackend E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_c_int00 E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_TSK_config E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_OBJ_table E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
HWI_A_VECS E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_FXN_F_nop E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_CLK_enableTimer E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_CLK_D_prd E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
IDL_D_calibrate E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_TSK E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_KNL_run E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
LNK_dspFrameRequestMask E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
CLK_F_isr E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
PIP_D_tabbeg E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
TRC_cinit E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_UTL_halt E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_MEM_init E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
RTA_F_dispatch E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_TSK_startup E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_TSK_setup E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_KNL_queues E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
CLK_A_TABBEG E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
LNK_F_dataPump E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
TSK_VEXITFXN E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
HWI_F_dispatch E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_RTDX_Poll E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_TSK_init E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
IDL_D_busyObj E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_TSK_exit E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
SWI_F_enable E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
FXN_F_run E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_HSRTDX_rec E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_GBL_getVersion E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_CLK_inputClock E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
GBL_initdone E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_HWI_dispatchTab E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
LNK_dspFrameReadyMask E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
IDL_F_busy E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Configuration4cfg.obj
_printf E:\\CCStudio_v3.3\\MyProjects\\tutorial\\trace\\64x\\Li2\\Debug\\Probieren.obj
>> error: symbol referencing errors - './Debug/Li2.out' not built
>> Compilation failure
Build Complete,2 Errors, 23 Warnings, 0 Remarks.
And also in forum said Tim to someone that include the BIOS-generated linker command file.
Can somebody tell me how can i include the BIOS-generated command file?
Best Greeting
Li,Liangjie