This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: GPIO wakeup

Part Number: PROCESSOR-SDK-AM335X


Tool/software: Linux

Hi

Basically i am using custom beagle bone black with latest TI SDK
i am able to put the CPU in sleep mode(standby,mem) and i can wake up from tty terminal key press.
but i am unable to wake up the CPU from a gpio pin can you please let me know the dts file changes in order to wake up the cpu from a gpio pin toggle.
bellow are the changes done by me

BUT BELLOW CHANGES WORKS FINE I AM ABLE TO WAKE UP using GPIO0_7

keys: wakeup_keys@0 {
compatible = "gpio-keys";
#address-cells = <1>;
#size-cells = <0>;
autorepeat;

test@0 {
label = "P8-pin24";
linux,code = <155>;
gpios = <&gpio0 7 GPIO_ACTIVE_LOW>;
gpio-key,wakeup;
};

};

since i need 2 gpio pins to wake up the CPU hence i added extra pin after which i cannot wake from any gpio pin 

NOT WORKING
--------------------

keys: wakeup_keys@0 {
compatible = "gpio-keys";
#address-cells = <1>;
#size-cells = <0>;
autorepeat;
    test@0 {
    label = "P8-pin24";
    linux,code = <155>;
    gpios = <&gpio0 7 GPIO_ACTIVE_LOW>;
    gpio-key,wakeup;
    };
    test@1 {
    label = “P9-pin23";
    linux,code = <155>;
    gpios = <&gpio0 27 GPIO_ACTIVE_LOW>;
    gpio-key,wakeup;
    };
};

my dmesg output
[ 0.572319] of_get_named_gpiod_flags: parsed 'gpios' property of node '/wakeup_keys@0/test@0[0]' - status (0)
[ 0.572357] of_get_named_gpiod_flags: parsed 'gpios' property of node '/wakeup_keys@0/test@1[0]' - status (0)
[ 0.572775] input: wakeup_keys@0 as /devices/platform/wakeup_keys@0/input/input0

--------------------------------

can you please let me know why i am not able to wake up from any gpio after i put CPU in sleep mode after i add bellow changes in the dts file but if i remove this i can wake up using gpio0_7

test@1 {
label = “P9-pin23";
linux,code = <155>;
gpios = <&gpio0 27 GPIO_ACTIVE_LOW>;
gpio-key,wakeup;
};

Regards