Part Number: TMDSICE3359
Tool/software: TI-RTOS
Hello,
I am using Processor SDK RTOS and have the Ethernetip_adapter application running on my ICE board.It has Ethernet IP Adapter application loaded in it via CCS.
The following softwares are installed.
- processor_sdk_rtos_am335x_3_03_00_04
- PRU-ICSS-EthernetIP_Adapter_01.00.02.00
- xdctools_3_32_01_22_core
- edma3_lld_2_12_03_27
The ethernet/ip adapter application is running on the Board and is able to communicate with the Molex EIP tool.
I want to transfer thIs data coming into Ethernet port to the UART.
what will be the specific steps to carry out the given task>